This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:ev-cog-ad3029lz:help_support [21 Dec 2017 09:33] Pranit Jadhav |
resources:eval:user-guides:ev-cog-ad3029lz:help_support [03 Jan 2021 21:55] Robin Getz fix links |
||
---|---|---|---|
Line 17: | Line 17: | ||
* The first thing to try in this case, is to [[resources:eval:user-guides:ev-cog-ad3029lz:tools:hardware_usb|drag and drop]] a known good .HEX or .BIN program into flash.(something with quick visible indicators works best) | * The first thing to try in this case, is to [[resources:eval:user-guides:ev-cog-ad3029lz:tools:hardware_usb|drag and drop]] a known good .HEX or .BIN program into flash.(something with quick visible indicators works best) | ||
* If drag and drop is not working, it may be necessary to erase the flash. To do so: | * If drag and drop is not working, it may be necessary to erase the flash. To do so: | ||
- | - Download and install the CrossCore Serial Flash Programmer from here: [[http://www.analog.com/en/design-center/processors-and-dsp/evaluation-and-development-software/crosscore-serial-flash-programmer.html#dsp-overview]]. | + | - Download and install the CrossCore Serial Flash Programmer from here: [[adi>en/design-center/processors-and-dsp/evaluation-and-development-software/crosscore-serial-flash-programmer.html#dsp-overview]]. |
- Make sure that the USB is connected and on UART header (P8) 1 & 2 and 7 & 8 are shorted. | - Make sure that the USB is connected and on UART header (P8) 1 & 2 and 7 & 8 are shorted. | ||
- Power cycle the EV-COG-AD3029LZ board while holding down the boot switch. | - Power cycle the EV-COG-AD3029LZ board while holding down the boot switch. |