This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ev-cog-ad3029lz:help_support [12 Aug 2017 08:28] – [What to do When Things Go Wrong] Pranit Jadhav | resources:eval:user-guides:ev-cog-ad3029lz:help_support [03 Jan 2021 21:55] (current) – fix links Robin Getz | ||
---|---|---|---|
Line 17: | Line 17: | ||
* The first thing to try in this case, is to [[resources: | * The first thing to try in this case, is to [[resources: | ||
* If drag and drop is not working, it may be necessary to erase the flash. To do so: | * If drag and drop is not working, it may be necessary to erase the flash. To do so: | ||
- | - Download and install the CrossCore Serial Flash Programmer from here: [[http:// | + | - Download and install the CrossCore Serial Flash Programmer from here: [[adi>en/ |
- Make sure that the USB is connected and on UART header (P8) 1 & 2 and 7 & 8 are shorted. | - Make sure that the USB is connected and on UART header (P8) 1 & 2 and 7 & 8 are shorted. | ||
- Power cycle the EV-COG-AD3029LZ board while holding down the boot switch. | - Power cycle the EV-COG-AD3029LZ board while holding down the boot switch. | ||
Line 27: | Line 27: | ||
- Not receiving/ | - Not receiving/ | ||
* Make sure that the UART header (P8) is positioned in the correct destination to transmit/ | * Make sure that the UART header (P8) is positioned in the correct destination to transmit/ | ||
+ | * JH6 is shorted. | ||
| | ||
This is just a brief self-help guide to troubleshooting common issues. | This is just a brief self-help guide to troubleshooting common issues. |