This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:cn0507-network-analyzer:sw_setup:start [06 Sep 2019 08:50] Jhake Zebedee Aquino |
resources:eval:user-guides:cn0507-network-analyzer:sw_setup:start [14 Jan 2021 05:12] Robin Getz user interwiki links |
||
---|---|---|---|
Line 2: | Line 2: | ||
===== Firmware ===== | ===== Firmware ===== | ||
- Download the hex file from the CN-0507 product page. | - Download the hex file from the CN-0507 product page. | ||
- | - If running an operating system older than Windows 10, install serial driver as in **[[https://wiki.analog.com/resources/eval/user-guides/EVAL-ADICUP3029/tools/keil_iar_support#how_to_use_EVAL-ADICUP3029_with_iar|1. Install mBed windows serial driver...]]** | + | - If running an operating system older than Windows 10, install serial driver as in **[[/resources/eval/user-guides/EVAL-ADICUP3029/tools/keil_iar_support#how_to_use_EVAL-ADICUP3029_with_iar|1. Install mBed windows serial driver...]]** |
- You should see DAPLINK in your list of drives. {{:resources:eval:user-guides:cn0507-network-analyzer:sw_setup:daplink.png?nolink|}} | - You should see DAPLINK in your list of drives. {{:resources:eval:user-guides:cn0507-network-analyzer:sw_setup:daplink.png?nolink|}} | ||
- Copy the hex file to the DAPLINK drive to load the firmware to the EVAL-ADICUP3029. Note that the DAPLINK drive will disappear for a moment, then reappear after loading the firmware. | - Copy the hex file to the DAPLINK drive to load the firmware to the EVAL-ADICUP3029. Note that the DAPLINK drive will disappear for a moment, then reappear after loading the firmware. |