Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:circuits-from-the-lab:eval-adxrs290-pmdz [27 Jan 2023 09:23] – Replaced the obsolete Kuiper Linux page link Joyce Velasco | resources:eval:user-guides:circuits-from-the-lab:eval-adxrs290-pmdz [03 Mar 2023 08:13] (current) – updated the design files download link Joyce Velasco |
---|
====== ADXRS290 Gyroscope PMOD Demo ====== | ====== ADXRS290 Gyroscope PMOD Demo ====== |
| |
The [[ADI>EVAL-ADXRS290-PMDZ]] is a simple Pmod form-factor evaluation board for the ADXRS290, a high-performance MEMS pitch-and-roll (dual-axis in-plane) angular rate sensor (gyroscope) designed for use in stabilization applications. | The [[ADI>EVAL-ADXRS290-PMDZ]] is a simple Pmod form-factor evaluation board for the [[adi>ADXRS290]], a high-performance MEMS pitch-and-roll (dual-axis in-plane) angular rate sensor (gyroscope) designed for use in stabilization applications. |
\\ | \\ |
| |
| |
* **Software** | * **Software** |
* [[:resources:tools-software/linux-software/kuiper-linux |Kuiper Images]] | * [[:resources:tools-software:linux-software:kuiper-linux |Kuiper Images]] |
| |
| |
==== Loading Image on SD Card ==== | ==== Loading Image on SD Card ==== |
| |
In order to control the **EVAL-ADXRS290-PMDZ** from the Raspberry Pi, you will need to install ADI Kuiper Linux on an SD card. Complete instructions, including where to download the SD card image, how to write it to the SD card, and how to configure the system are provided at **[[:resources:tools-software/linux-software/kuiper-linux |Kuiper Images]]**. | In order to control the **EVAL-ADXRS290-PMDZ** from the Raspberry Pi, you will need to install ADI Kuiper Linux on an SD card. Complete instructions, including where to download the SD card image, how to write it to the SD card, and how to configure the system are provided at **[[:resources:tools-software:linux-software:kuiper-linux |Kuiper Images]]**. |
\\ | \\ |
Write the image and follow the system configuration procedure. | Write the image and follow the system configuration procedure. |
==== Configuring the SD Card ==== | ==== Configuring the SD Card ==== |
Follow the Hardware Configuration procedure under **Preparing the Image: Raspberry Pi** in the [[:resources:tools-software/linux-software/kuiper-linux |Kuiper Images]] page, substituting the following lines in **config.txt**: | Follow the Hardware Configuration procedure under **Preparing the Image: Raspberry Pi** in the [[:resources:tools-software:linux-software:kuiper-linux |Kuiper Images]] page, substituting the following lines in **config.txt**: |
| |
<code> | <code> |
| |
<WRAP round 80% download> | <WRAP round 80% download> |
| [[adi>media/en/evaluation-documentation/evaluation-design-files/eval-adxrs290-pmdz-designsupport.zip|EVAL-ADXRS20-PMDZ Design & Integration Files]] |
* {{ :resources:eval:user-guides:circuits-from-the-lab:eval-adxrs290-pmdz:02_065300a_top.pdf | Schematics}} | * Schematic |
* {{ :resources:eval:user-guides:circuits-from-the-lab:eval-adxrs290-pmdz:08_065300a.pdf | PCB Layout}} | * PCB Layout |
* {{ :resources:eval:user-guides:circuits-from-the-lab:eval-adxrs290-pmdz:20-065300-01a.zip | Allegro Project}} | * Bill of Materials |
* {{ :resources:eval:user-guides:circuits-from-the-lab:eval-adxrs290-pmdz:bom.zip |Bill of Materials}} | * Allegro Project |
</WRAP> | </WRAP> |
| |
* [[https://github.com/analogdevicesinc/no-OS/wiki|ADXRS290 No-OS Build Instruction Guide]] | * [[https://github.com/analogdevicesinc/no-OS/wiki|ADXRS290 No-OS Build Instruction Guide]] |
* [[https://github.com/analogdevicesinc/no-OS/tree/master/projects/adxrs290-pmdz|ADXRS290 No-OS Drivers]] | * [[https://github.com/analogdevicesinc/no-OS/tree/master/projects/adxrs290-pmdz|ADXRS290 No-OS Drivers]] |
* [[:resources:tools-software/linux-software/kuiper-linux |Kuiper Images]] | * [[:resources:tools-software:linux-software:kuiper-linux |Kuiper Images]] |
| |
=====Registration===== | =====Registration===== |