This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:circuits-from-the-lab:eval-adxl355-pmdz [12 Apr 2023 02:40] – [Additional Information and Useful Links] Trisha Cabildo | resources:eval:user-guides:circuits-from-the-lab:eval-adxl355-pmdz [20 Apr 2023 08:03] (current) – update Trisha Cabildo | ||
---|---|---|---|
Line 232: | Line 232: | ||
To set up the circuit for evaluation, consider the following steps: | To set up the circuit for evaluation, consider the following steps: | ||
- Connect the **P9** of the **PMOD to Raspberry Pi Interposer** board at the male header GPIO pin connector of the **Raspberry Pi** as shown below. {{ : | - Connect the **P9** of the **PMOD to Raspberry Pi Interposer** board at the male header GPIO pin connector of the **Raspberry Pi** as shown below. {{ : | ||
- | - Connect the ** [[ADI> | + | - Connect the ** [[ADI> |
- Burn the SD card with the proper ADI Kuiper Linux image. Insert the burned SD card on the designated slot on the RPi. | - Burn the SD card with the proper ADI Kuiper Linux image. Insert the burned SD card on the designated slot on the RPi. | ||
- Connect the system to a monitor using an HDMI cable through the mini HDMI connector on the RPi. | - Connect the system to a monitor using an HDMI cable through the mini HDMI connector on the RPi. |