This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:eval-adpd410x [22 Jun 2022 06:25] – Angelo Nikko Catapang | resources:eval:user-guides:circuits-from-the-lab:eval-adpd410x [22 Jun 2022 06:31] – Angelo Nikko Catapang | ||
---|---|---|---|
Line 34: | Line 34: | ||
=== LED Supply Voltage (JP1) Solder Positions === | === LED Supply Voltage (JP1) Solder Positions === | ||
^ Correct Shunt Position ^ Layout Picture | ^ Correct Shunt Position ^ Layout Picture | ||
- | | Shorted Pin 1 and 2 | {{ : | + | | Shorted Pin 2 and 3 | {{ : |
=== LED Driver Connection P9, P11, P13, P15, P17, P19, P22, P24 === | === LED Driver Connection P9, P11, P13, P15, P17, P19, P22, P24 === | ||
Line 88: | Line 88: | ||
==== Using CrossCore Embedded Studio ==== | ==== Using CrossCore Embedded Studio ==== | ||
- | - Acquire a copy of the project source files of the EVAL-ADPD410X-ARDZ by downloading the source files directly from the repository at [[repo> | + | - Acquire a copy of the project source files of the EVAL-ADPD410X-ARDZ by downloading the source files directly from the repository at [[repo> |
- Open CrossCore Embedded Studio and import the project into your workspace, as detailed in the [[: | - Open CrossCore Embedded Studio and import the project into your workspace, as detailed in the [[: | ||
- Once ready, you can opt to generate your own .hex file and use the first method to program the **[[ADI> | - Once ready, you can opt to generate your own .hex file and use the first method to program the **[[ADI> | ||
=== CrossCore Project Header File Configuration === | === CrossCore Project Header File Configuration === | ||
- | * Select which board the project will support when built using [[https:// | + | * Select which board the project will support when built using [[https:// |
* For EVAL-ADPD4100-ARDZ\\ {{: | * For EVAL-ADPD4100-ARDZ\\ {{: | ||
* For EVAL-ADPD4101-ARDZ\\ {{: | * For EVAL-ADPD4101-ARDZ\\ {{: | ||
- | You can configure the default timeslots and other settings of the [[ADI> | + | You can configure the default timeslots and other settings of the [[ADI> |
* You can set the default number of active timeslots and output data rate.\\ {{: | * You can set the default number of active timeslots and output data rate.\\ {{: | ||
* Initial timeslot settings are configured using the **adpd410x_timeslot_init** data structure, as shown below:\\ {{: | * Initial timeslot settings are configured using the **adpd410x_timeslot_init** data structure, as shown below:\\ {{: |