Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:circuits-from-the-lab:eval-adpd410x [22 Jun 2022 06:25]
Angelo Nikko Catapang
resources:eval:user-guides:circuits-from-the-lab:eval-adpd410x [22 Jun 2022 06:31] (current)
Angelo Nikko Catapang
Line 34: Line 34:
 === LED Supply Voltage (JP1) Solder Positions === === LED Supply Voltage (JP1) Solder Positions ===
 ^ Correct Shunt Position ^ Layout Picture ​                                                                      ^ ^ Correct Shunt Position ^ Layout Picture ​                                                                      ^
-| Shorted Pin 1 and 2    | {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​jp1_5v.png?​nolink&​100 |}} |+| Shorted Pin 2 and 3    | {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​jp1_5v.png?​nolink&​100 |}} |
  
 === LED Driver Connection P9, P11, P13, P15, P17, P19, P22, P24 === === LED Driver Connection P9, P11, P13, P15, P17, P19, P22, P24 ===
Line 88: Line 88:
  
 ==== Using CrossCore Embedded Studio ==== ==== Using CrossCore Embedded Studio ====
-  - Acquire a copy of the project source files of the EVAL-ADPD410X-ARDZ by downloading the source files directly from the repository at [[repo>​EVAL-ADICUP3029/​tree/​dev/cn0567/projects/ADuCM3029_demo_cn0567]] or you can clone the entire [[https://​github.com/​analogdevicesinc/​EVAL-ADICUP3029 | EVAL-ADICUP3029 repository]] and check the projects folder for ADuCM3029_demo_cn0567.+  - Acquire a copy of the project source files of the EVAL-ADPD410X-ARDZ by downloading the source files directly from the repository at [[repo>​EVAL-ADICUP3029/​tree/​master/projects/ADuCM3029_demo_adpd410x]] or you can clone the entire [[https://​github.com/​analogdevicesinc/​EVAL-ADICUP3029 | EVAL-ADICUP3029 repository]] and check the projects folder for ADuCM3029_demo_adpd410x.
   - Open CrossCore Embedded Studio and import the project into your workspace, as detailed in the [[:​resources:​eval:​user-guides:​eval-adicup3029:​tools:​cces_user_guide]]. This allows you to edit the software to fit your requirements. <WRAP important>​If this is your first time using CrossCore Embedded Studio, check the [[:​resources:​eval:​user-guides:​eval-adicup3029:​tools:​cces_user_guide | user guide]] to get started.</​WRAP>​   - Open CrossCore Embedded Studio and import the project into your workspace, as detailed in the [[:​resources:​eval:​user-guides:​eval-adicup3029:​tools:​cces_user_guide]]. This allows you to edit the software to fit your requirements. <WRAP important>​If this is your first time using CrossCore Embedded Studio, check the [[:​resources:​eval:​user-guides:​eval-adicup3029:​tools:​cces_user_guide | user guide]] to get started.</​WRAP>​
   - Once ready, you can opt to generate your own .hex file and use the first method to program the **[[ADI>​EVAL-ADICUP3029]]** or you can use a debug session by following the quickstart guide.   - Once ready, you can opt to generate your own .hex file and use the first method to program the **[[ADI>​EVAL-ADICUP3029]]** or you can use a debug session by following the quickstart guide.
  
 === CrossCore Project Header File Configuration === === CrossCore Project Header File Configuration ===
-  * Select which board the project will support when built using [[https://​github.com/​analogdevicesinc/​EVAL-ADICUP3029/​blob/​master/​projects/​ADuCM3029_demo_cn0567/​src/​app_config.h|app_config.h]].+  * Select which board the project will support when built using [[https://​github.com/​analogdevicesinc/​EVAL-ADICUP3029/​blob/​master/​projects/​ADuCM3029_demo_adpd410x/​src/​app_config.h|app_config.h]].
     * For EVAL-ADPD4100-ARDZ\\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​adpd4100_support.png?​nolink&​400|}}     * For EVAL-ADPD4100-ARDZ\\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​adpd4100_support.png?​nolink&​400|}}
     * For EVAL-ADPD4101-ARDZ\\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​adpd4101_support.png?​nolink&​400|}}     * For EVAL-ADPD4101-ARDZ\\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​adpd4101_support.png?​nolink&​400|}}
-You can configure the default timeslots and other settings of the [[ADI>​ADPD4100]] or [[ADI>​ADPD4101]] using [[https://​github.com/​analogdevicesinc/​EVAL-ADICUP3029/​blob/​master/​projects/​ADuCM3029_demo_cn0567/src/cn0567_config.h|cn0567_config.h]].+You can configure the default timeslots and other settings of the [[ADI>​ADPD4100]] or [[ADI>​ADPD4101]] using [[https://​github.com/​analogdevicesinc/​EVAL-ADICUP3029/​blob/​master/​projects/​ADuCM3029_demo_adpd410x/src/adpd410x_app_config.h|adpd410x_app_config.h]].
   * You can set the default number of active timeslots and output data rate.\\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​activetimeslots_odr.png?​nolink&​400|}}   * You can set the default number of active timeslots and output data rate.\\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​activetimeslots_odr.png?​nolink&​400|}}
   * Initial timeslot settings are configured using the **adpd410x_timeslot_init** data structure, as shown below:\\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​timeslot_datastructure.png?​nolink&​400|}}   * Initial timeslot settings are configured using the **adpd410x_timeslot_init** data structure, as shown below:\\ {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​timeslot_datastructure.png?​nolink&​400|}}
resources/eval/user-guides/circuits-from-the-lab/eval-adpd410x.txt · Last modified: 22 Jun 2022 06:31 by Angelo Nikko Catapang