This is an old revision of the document!
The EVAL-ADISIMU1-RPIZ allows multiple compatible IMU components (with the ADIS16IMU1/PCBZ and ADIS16IMU4/PCBZ breakout boards connector) to be connected to the Raspberry Pi. The following table outlines which IMU components can be directly mounted with the EVAL-ADISIMU1-RPIZ board
IMU Part Number | ADISIMU1 Connector | Mounting Location | Breakout Board Connector |
---|---|---|---|
ADIS16360 | P2 | Mounting Slot B | ADIS16IMU1/PCBZ |
ADIS16400 | P2 | Mounting Slot B | ADIS16IMU1/PCBZ |
ADIS16362 | P2 | Mounting Slot B | ADIS16IMU1/PCBZ |
ADIS16364 | P2 | Mounting Slot B | ADIS16IMU1/PCBZ |
ADIS16365 | P2 | Mounting Slot B | ADIS16IMU1/PCBZ |
ADIS16367 | P2 | Mounting Slot B | ADIS16IMU1/PCBZ |
ADIS16405 | P2 | Mounting Slot B | ADIS16IMU1/PCBZ |
ADIS16407 | P2 | Mounting Slot B | ADIS16IMU1/PCBZ |
ADIS16133 | P2 | Mounting Slot C | ADIS16IMU1/PCBZ |
ADIS16135 | P2 | Mounting Slot C | ADIS16IMU1/PCBZ |
ADIS16136 | P2 | Mounting Slot C | ADIS16IMU1/PCBZ |
ADIS16137 | P2 | Mounting Slot C | ADIS16IMU1/PCBZ |
ADIS16375 | P2 | Mounting Slot F | ADIS16IMU1/PCBZ |
ADIS16480 | P2 | Mounting Slot F | ADIS16IMU1/PCBZ |
ADIS16485 | P2 | Mounting Slot F | ADIS16IMU1/PCBZ |
ADIS16488A | P2 | Mounting Slot F | ADIS16IMU1/PCBZ |
ADIS16489 | P2 | Mounting Slot F | ADIS16IMU1/PCBZ |
ADIS16490 | P2 | Mounting Slot F | ADIS16IMU1/PCBZ |
ADIS16495 | P2 | Mounting Slot F | ADIS16IMU1/PCBZ |
ADIS16497 | P2 | Mounting Slot F | ADIS16IMU1/PCBZ |
ADIS16467 | P7 | Mounting Slot I | ADIS16IMU4/PCBZ |
ADIS16460 | P7 | Mounting Slot I | ADIS16IMU4/PCBZ |
ADIS16465 | P7 | Mounting Slot I | ADIS16IMU4/PCBZ |
The following video is a walkthrough for the unboxing experience and a guide for setting up the hardware to be ready for your own application development.
There are two ways you can mount components on the EVAL-ADISIMU1-RPIZ.
Any IMU can use the indirect method of connecting to the P3 header using the ribbon cable and it's corresponding breakout board. So the following sections are going to describe how to directly mount the compatible IMUs to the EVAL-ADISIMU1-RPIZ. Please see the pictures for device mounting hole locations.
There are four(4) mounting holes without any labels. These mounting holes are assigned to mount the EVAL-ADISIMU1-RPIZ to the Raspberry Pi host board. There are four(4) nylon screws and spacers provided in the kit, and these should be used for this purpose. The nominal diameter of the four(4) holes is 3.175mm.
MACHINE SCREWS IMPACT LOCAL MAGNETIC FIELDS
The machine screws in the EVAL-ADISIMU1-RPIZ kit are made out of stainless steel, which can have some moderate impact on magnetic fields, local to the IMU. For those whose application demands the best magnetometer performance offered by these IMUs, consider using plastic screws that will not impact the magnetic fields around the devices.
IMU Components
Mounting Materials
The image below shows the proper mounting of IMU's on Mounting Slot B.
IMU Components
Mounting Materials
Below is an example of proper mounting of IMU's on mounting hole C
IMU Components
Mounting Materials
Below is an image that show proper mounting of IMU's on mounting slot F.
IMU Components:
Mounting Materials
Below is an image that show proper mounting of IMU's on mounting slot I. Ensure that the machine screws are tightened on the bottom side of the board using the hex nuts as shown below:
The 40 pin Raspberry Pi connector of the EVAL-ADISIMU1-RPIZ mounts directly on top of the Raspberry Pi 4, or equivalents, 40 pin male headers.
Placing a shunt on this connector P1 provides power to the Real Time Clock (RTC) of the IMU's attached to connector P2
The board has a selectable power between +5V or +3.3V from the RPI. The default power supply is +3.3V unless otherwise stated in the datasheet of the IMU. The power to the IMU can be selected using connector P5.
It's critical to know the power supply required for the IMU you are using before changing this setting. If you power any IMU from 5V that was designed for 3.3V power, you will destroy the IMU and it will no longer function. This is a VERY EXPENSIVE mistake.
Power | Shunt Position |
---|---|
+5.0V | Pin 1 and Pin 2 |
+3.3V | Pin 2 and Pin 3 (Default Position) |
Header P6 allows for selectable sync signal to be used by the IMU's. It can be done by moving the shunt to select the source, either via RPI or an external source.
Sync | Shunt Position |
---|---|
RPI | Pin 1 and Pin 2 (Default Position) |
Ext | Pin 3 and Pin 4 |
This allows for an external sync signal to be used in the system by installing an SMA connector on pads of connector J1.
This test point provides connection to the +5V rail.
This test point provides connection to the +3.3V rail.
This test point provides connection to the ground.
This test point provides connection to the output of the DAC.
This test point provides connection to the output of the ADC.
EVAL-ADISIMU1-RPIZ Design & Integration Files
End of Document