Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:circuits-from-the-lab:eval-ad5593r-pmdz [20 Apr 2023 08:01] – update Trisha Cabildoresources:eval:user-guides:circuits-from-the-lab:eval-ad5593r-pmdz [02 May 2023 03:34] (current) – update images Trisha Cabildo
Line 242: Line 242:
 <note important>Make sure to download/update to the latest version of IIO-Oscilloscope found on this link[[https://github.com/analogdevicesinc/iio-oscilloscope/releases]]</note> <note important>Make sure to download/update to the latest version of IIO-Oscilloscope found on this link[[https://github.com/analogdevicesinc/iio-oscilloscope/releases]]</note>
   - Once done with the installation or an update of the latest IIO-Oscilloscope, open the application.  The user needs to supply a URI which will be used in the context creation of the IIO Oscilloscope and the instructions can be seen in the previous section.   - Once done with the installation or an update of the latest IIO-Oscilloscope, open the application.  The user needs to supply a URI which will be used in the context creation of the IIO Oscilloscope and the instructions can be seen in the previous section.
-  - Press refresh to display available IIO Devices, once ad5593r appeared, press connect. <fc #ff0000>**UPDATE PIC!!**</fc> +  - Press refresh to display available IIO Devices, once ad5593r appeared, press connect.  
-{{ resources:eval:user-guides:circuits-from-the-lab:cn0552:osc.png?200 | AD5593R Oscilloscope Configuration}}+{{ :resources:eval:user-guides:circuits-from-the-lab:ad5593r-pmod:5593_iio_connect.jpg?nolink&300 | AD5593R Oscilloscope Configuration}}
  
 === Debug Panel === === Debug Panel ===
  
-Below is the Debug panel of AD5593R wherein you can directly access the attributes of the device. <fc #ff0000>**UPDATE PIC!!**</fc> +Below is the Debug panel of AD5593R wherein you can directly access the attributes of the device.  
-{{ :resources:eval:user-guides:circuits-from-the-lab:cn0552:debug_panel.png?direct&400 | AD5593R Debug Panel}}+{{ :resources:eval:user-guides:circuits-from-the-lab:ad5593r-pmod:5593_debug.jpg?nolink&300 | AD5593R Debug Panel}}
  
 === DMM Panel === === DMM Panel ===
  
-Access the DMM panel to see the instantaneous reading of the input capacitances and the device temperature.  <fc #ff0000>**UPDATE PIC!!**</fc> +Access the DMM panel to see the instantaneous reading of the input capacitances and the device temperature.   
-{{ :resources:eval:user-guides:circuits-from-the-lab:cn0552:dmm_readings.png?direct&400 | AD5593R DMM Panel }}+{{ :resources:eval:user-guides:circuits-from-the-lab:ad5593r-pmod:5593_dmm.jpg?nolink&300 | AD5593R DMM Panel}}
  
 ==== PyADI-IIO ==== ==== PyADI-IIO ====
Line 269: Line 269:
 Press enter and you will get these readings. Press enter and you will get these readings.
  
-{{:resources:eval:user-guides:circuits-from-the-lab:cn0552:python_script.png?500}} <fc #ff0000>**UPDATE PIC!!**</fc>+{{ :resources:eval:user-guides:circuits-from-the-lab:ad5593r-pmod:5593_pyadi.jpg?nolink&600 |AD5593R }}
  
 <WRAP round 80% download> <WRAP round 80% download>
resources/eval/user-guides/circuits-from-the-lab/eval-ad5593r-pmdz.txt · Last modified: 02 May 2023 03:34 by Trisha Cabildo