Wiki

This version is outdated by a newer approved version.DiffThis version (11 Mar 2024 07:46) was approved by Joyce Velasco.

This is an old revision of the document!


CN0588 User Guide

Overview

The CN0588 is a MEMS-based IEPE vibration sensor optimized for condition-based monitoring (CbM) applications. This solution has a constant current supply of 4 mA and a DC voltage bias ranging from around 8.75 V to 14.75 V.


Since Piezoelectric sensors are predominantly used in CbM applications, IEPE is the de facto standard in CbM vibration sensing ecosystem. The IEPE interface, also commercially known as ICP, is a 2-wire protocol, signal and ground. In this protocol a data logger supplies a constant current via the signal line to the vibration sensor and the sensor modulates the voltage according to the measurand, typically between 10 V to 30 V. This reference design enables a direct IEPE piezoelectric sensor replacement with benefits of high bandwidth, temperature stability and ultralow noise MEMS accelerometers. This allows customers to easily evaluate an IEPE MEMS accelerometer solution for CbM applications on the same ICP piezoelectric sensor platform.

Features

  • Mechanically enclosed and machine mountable
  • IEPE interface to retrofit into existing infrastructures
  • Power and data over a single wire, power comes from host
  • Within ±3 dB response up to 10 kHz frequency range
  • Sensor resonant frequency around 12.5 kHz
  • Designed for 60 mV/g sensitivity


Applications

  • Predictive Maintenance
  • Vibration Analysis
  • Condition Monitoring
  • Industrial Machinery Control


Block Diagram




Hardware Setup

Equipment Needed

  • EVAL-CN0588-EBZ
  • Current Source (e.g., Keithley 6220), or an IEPE-compatible DAQ such as the CN0582, CN0540, CN0579
  • Vibration Shaker (e.g., King Design 9363-ED-2F4K-5N)
  • Signal Generator
  • SMA Cable (10-32)
  • BNC Cable

Setting up the Hardware



  1. Mount the EVAL-CN0588-EBZ to the vibration shaker.
  2. Connect the SMA cable to the EVAL-CN0588-EBZ.
  3. Connect the other end of the SMA cable to the current source.
  4. Set the output constant current to 4 mA, and controlled voltage to 26 V.
  5. Connect the BNC cable to the vibration shaker.
  6. Connect the other end of the BNC cable to the signal generator (output).
  7. Set the frequency settings to your requirement.
  8. The voltage of the current source is the output. Without an external acceleration, the IEPE output should be around 12 V.


The EVAL-CN0588-EBZ is ready for experiment.


Sample Measurements


Using CN0588 with the CN0582 Quad-Channel IEPE DAQ

For applications requiring 4 channels, the CN0582 is the recommended IEPE vibration measurement equipment to be paired with the CN0588. Follow below procedure to set up the system for evaluation.


Equipment Needed

  • EVAL-CN0588-EBZ
  • EVAL-CN0582-USBZ
  • Host PC (Windows 10)
  • Vibration Shaker (e.g., King Design 9363-ED-2F4K-5N)
  • Reference Sensor (PCBM352C67)
  • Power Supply (19 V)
  • USB Type-C Cable
  • Two (2) SMA Cables
  • BNC Cable


This measurement demonstration uses the EVAL-CN0582-USBZ as IEPE-compatible vibration measurement equipment, and requires the CN0582 Evaluation Software to be installed.

For instructions on how to obtain and install the software, visit the CN0582 User Guide

  1. Mount the EVAL-CN0588-EBZ to the vibration shaker.
  2. Connect the EVAL-CN0582-USBZ to the vibration shaker using a BNC connector.
  3. By using SMA connector, connect the Piezo reference sensor of the vibration shaker to Channel 0.
  4. Attach another SMA connector from the EVAL-CN0588-EBZ going to Channel 1 of the EVAL-CN0582-USBZ.
  5. Power up the EVAL-CN0582-USBZ by connecting the Type C end of the USB cable to the board and the other end to the host PC.

    The RED and GREEN LED should light, indicating proper power up.

  6. Turn on the vibration shaker by plugging in the 19 V power supply.
  7. Ready the shaker by clicking the tune button. Two (2) green LEDs must light up.
  8. Download and install the CN0582 Evaluation Software.

    Only the GREEN LED should light up on the board during installation. This indicates successful firmware upload.

  9. Follow the installation prompts until the main window of the GUI appears.
  10. On the GUI dashboard, navigate to the left and click 'Vibration Testing' to launch the window.
  11. Toggle ON the current source in the Reference & DUT Sensor Setup Section (5).
  12. Set the acceleration sensitivity and the sensor DC bias (mV) using the following values:

    Reference

    • Current Source = ON
    • Sensitivity = 100 mV/g
    • Sensor DC Bias = 10700 mV

    DUT

    • Enable = ON
    • Current Source = ON
    • Sensitivity = 60 mV/g
    • Sensor DC Bias = 8000 to 13000 mV
  13. Adjust the frequency settings to your requirements.
  14. Connect the other end of the BNC cable to the EVAL-CN0582-USBZ (J6).
  15. Click Start to launch the test. Then wait for it to finish.



The CN0588's IEPE interface makes it suitable to be used with different IEPE-compatible data acquisition systems. Analog Devices has various IEPE reference designs that users can readily evaluate and prototype with.

For CbM applications requiring one channel measurement, the CN0540 24-Bit IEPE data acquisition system is recommended.

For applications requiring Arduino form-factor, the CN0579 is the suggested IEPE vibration sensor measurement system to use with the CN0588.



Resources

Design & Integration Files

EVAL-CN0588-EBZ Design & Integration Files

  • Schematics
  • PCB Layout
  • Bill of Materials
  • Allegro Project

Registration

Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware. Register to receive all these great benefits and more!

Help and Support

For questions and more information about this product, connect with us through the Analog Devices Engineer Zone.



End of Document

resources/eval/user-guides/circuits-from-the-lab/cn0588.1709712421.txt.gz · Last modified: 06 Mar 2024 09:07 by Ace Alcid