Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
Next revision Both sides next revision
resources:eval:user-guides:circuits-from-the-lab:cn0585 [18 May 2023 12:53]
Paul Pop [Reference Demos & Software]
resources:eval:user-guides:circuits-from-the-lab:cn0585 [29 May 2023 10:36]
Paul Pop tables updates
Line 363: Line 363:
  
 Remote data streaming to and from hardware is made available through system object interfaces, which are unique for each component or platform. ​ Remote data streaming to and from hardware is made available through system object interfaces, which are unique for each component or platform. ​
-The hardware interfacing system objects provide a since class to both configure a given platform and move data back and forth from the device.+The hardware interfacing system objects provide a class to both configure a given platform and move data back and forth from the device.
 After running the [[https://​github.com/​analogdevicesinc/​HighSpeedConverterToolbox/​blob/​cn0585_v1/​test/​CN0585StreamingTest.m | CN0585StreamingTest.m ]] example The following window will pop up:  After running the [[https://​github.com/​analogdevicesinc/​HighSpeedConverterToolbox/​blob/​cn0585_v1/​test/​CN0585StreamingTest.m | CN0585StreamingTest.m ]] example The following window will pop up: 
  
Line 382: Line 382:
 |< 100% 15% 5% 80% >| |< 100% 15% 5% 80% >|
 ^ Interface signal name ^ Width ^ Description ^ ^ Interface signal name ^ Width ^ Description ^
-CN0585 ADC Data 0 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design. | +IP Data 0 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design. | 
-CN0585 ADC Data 1 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design. | +IP Data 1 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design. | 
-CN0585 ADC Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. | +IP Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. | 
-CN0585 ADC Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. |+IP Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. |
 | IP Valid Tx Data IN  | 1  | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. ​ | | IP Valid Tx Data IN  | 1  | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. ​ |
 | CN0585 DAC Data 0 OUT | 16 | AD3552R_0 DAC 0 channel data. To be used as input into the AD3552R interface IP. | | CN0585 DAC Data 0 OUT | 16 | AD3552R_0 DAC 0 channel data. To be used as input into the AD3552R interface IP. |
Line 391: Line 391:
 | CN0585 DAC Data 2 OUT | 16 | AD3552R_1 DAC 0 channel data. To be used as input into the AD3552R interface IP. | | CN0585 DAC Data 2 OUT | 16 | AD3552R_1 DAC 0 channel data. To be used as input into the AD3552R interface IP. |
 | CN0585 DAC Data 3 OUT | 16 | AD3552R_1 DAC 1 channel data. To be used as input into the AD3552R interface IP. | | CN0585 DAC Data 3 OUT | 16 | AD3552R_1 DAC 1 channel data. To be used as input into the AD3552R interface IP. |
-| IP Data Valid OUT     | 1 | Output signal that has to be logic '​1'​ for a clock cycle period when the data starts to be valid. ​ | +| IP Load Tx Data OUT   | 1 | Custom IP output signal used to notify the design that the IP is ready to receive new input data. Output signal that has to be logic '1' for a clock cycle period when the data starts to be valid |
-| IP Load Tx Data OUT   | 1 | Custom IP output signal used to notify the design that the IP is ready to receive new input data. The duration must be 1 clock cycle. |+
  
  
Line 399: Line 398:
 {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0585:​tx_configuration_lldk.png?​600 }} {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0585:​tx_configuration_lldk.png?​600 }}
  
-== Recieve ​reference design (Rx) ==+== Receive ​reference design (Rx) ==
 |< 100% 15% 5% 80% >| |< 100% 15% 5% 80% >|
 ^ Interface signal name ^ Width ^ Description ^ ^ Interface signal name ^ Width ^ Description ^
-IP Data 0 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design. | +CN0585 ADC Data 0 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design. | 
-IP Data 1 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design. | +CN0585 ADC Data 1 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design. | 
-IP Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. | +CN0585 ADC Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. | 
-IP Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. | +CN0585 ADC Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. | 
-| IP Valid Tx Data IN | 1 | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. ​ |+| IP Valid Rx Data IN | 1 | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. ​ |
 | IP Data 0 OUT | 16 | ADAQ23876 ADC 0 channel data. To be used as input for the ADC CPAK IP. | | IP Data 0 OUT | 16 | ADAQ23876 ADC 0 channel data. To be used as input for the ADC CPAK IP. |
 | IP Data 1 OUT | 16 | ADAQ23876 ADC 1 channel data. To be used as input for the ADC CPAK IP. | | IP Data 1 OUT | 16 | ADAQ23876 ADC 1 channel data. To be used as input for the ADC CPAK IP. |
Line 419: Line 418:
  
  
-== Transmit and Recieve ​reference design (Tx & Rx) ==+== Transmit and Receive ​reference design (Tx & Rx) ==
 |< 100% 15% 5% 80% >| |< 100% 15% 5% 80% >|
 ^ Interface signal name ^ Width ^ Description ^ ^ Interface signal name ^ Width ^ Description ^
resources/eval/user-guides/circuits-from-the-lab/cn0585.txt · Last modified: 25 Sep 2023 21:45 by Rukiye Guldali