Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision Both sides next revision
resources:eval:user-guides:circuits-from-the-lab:cn0584 [29 May 2023 10:44]
Paul Pop [Additional Information and Useful Links]
resources:eval:user-guides:circuits-from-the-lab:cn0584 [31 May 2023 10:39]
Paul Pop [MATLAB and Simulink]
Line 315: Line 315:
  
 ==== MATLAB and Simulink ==== ==== MATLAB and Simulink ====
- 
 <WRAP round  download> ​ <WRAP round  download> ​
 Required MATLAB Add-Ons: ​ Required MATLAB Add-Ons: ​
Line 353: Line 352:
 |< 100% 15% 5% 80% >| |< 100% 15% 5% 80% >|
 ^ Interface signal name ^ Width ^ Description ^ ^ Interface signal name ^ Width ^ Description ^
-CN0584 ADC Data 0 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design. | +IP Data 0 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design. | 
-CN0584 ADC Data 1 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design. | +IP Data 1 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design. | 
-CN0584 ADC Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. | +IP Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. | 
-CN0584 ADC Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. |+IP Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. |
 | IP Valid Tx Data IN  | 1  | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. ​ | | IP Valid Tx Data IN  | 1  | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. ​ |
-CN0584 ​DAC Data 0 OUT | 16 | AD3552R_0 DAC 0 channel data. To be used as input into the AD3552R interface IP. | +CN0585 ​DAC Data 0 OUT | 16 | AD3552R_0 DAC 0 channel data. To be used as input into the AD3552R interface IP. | 
-CN0584 ​DAC Data 1 OUT | 16 | AD3552R_0 DAC 1 channel data. To be used as input into the AD3552R interface IP. | +CN0585 ​DAC Data 1 OUT | 16 | AD3552R_0 DAC 1 channel data. To be used as input into the AD3552R interface IP. | 
-CN0584 ​DAC Data 2 OUT | 16 | AD3552R_1 DAC 0 channel data. To be used as input into the AD3552R interface IP. | +CN0585 ​DAC Data 2 OUT | 16 | AD3552R_1 DAC 0 channel data. To be used as input into the AD3552R interface IP. | 
-CN0584 ​DAC Data 3 OUT | 16 | AD3552R_1 DAC 1 channel data. To be used as input into the AD3552R interface IP. +CN0585 ​DAC Data 3 OUT | 16 | AD3552R_1 DAC 1 channel data. To be used as input into the AD3552R interface IP. | 
-| IP Data Valid OUT     | 1 | Output signal that has to be logic '​1'​ for a clock cycle period when the data starts to be valid.  ​+| IP Load Tx Data OUT   | 1 | Custom IP output signal used to notify the design that the IP is ready to receive new input data. Output signal that has to be logic '1' for a clock cycle period when the data starts to be valid |
-| IP Load Tx Data OUT   | 1 | Custom IP output signal used to notify the design that the IP is ready to receive new input data. The duration must be 1 clock cycle. |+
  
  
Line 373: Line 371:
 |< 100% 15% 5% 80% >| |< 100% 15% 5% 80% >|
 ^ Interface signal name ^ Width ^ Description ^ ^ Interface signal name ^ Width ^ Description ^
-IP Data 0 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design. | +CN0585 ADC Data 0 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design. | 
-IP Data 1 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design. | +CN0585 ADC Data 1 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design. | 
-IP Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. | +CN0585 ADC Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. | 
-IP Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. | +CN0585 ADC Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. | 
-| IP Valid Tx Data IN | 1 | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. ​ |+| IP Valid Rx Data IN | 1 | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. ​ |
 | IP Data 0 OUT | 16 | ADAQ23876 ADC 0 channel data. To be used as input for the ADC CPAK IP. | | IP Data 0 OUT | 16 | ADAQ23876 ADC 0 channel data. To be used as input for the ADC CPAK IP. |
 | IP Data 1 OUT | 16 | ADAQ23876 ADC 1 channel data. To be used as input for the ADC CPAK IP. | | IP Data 1 OUT | 16 | ADAQ23876 ADC 1 channel data. To be used as input for the ADC CPAK IP. |
Line 397: Line 395:
 | IP Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. | | IP Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. |
 | IP Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. | | IP Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. |
-CN0584 ​ADC Data 0 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design. | +CN0585 ​ADC Data 0 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_0 IP ADC DATA port in the ADI reference design. | 
-CN0584 ​ADC Data 1 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design. | +CN0585 ​ADC Data 1 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_1 IP ADC DATA port in the ADI reference design. | 
-CN0584 ​ADC Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. | +CN0585 ​ADC Data 2 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_2 IP ADC DATA port in the ADI reference design. | 
-CN0584 ​ADC Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. |+CN0585 ​ADC Data 3 IN | 16 | Custom IP data input signal. This signal is connected to the AXI_LTC2387_3 IP ADC DATA port in the ADI reference design. |
 | IP Valid Rx Data IN | 1 | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. | | IP Valid Rx Data IN | 1 | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. |
 | IP Valid Tx Data IN | 1 | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. | | IP Valid Tx Data IN | 1 | Input signal that has logic 1 value for a clock cycle period when the data starts to be valid. |
Line 407: Line 405:
 | IP Data 2 OUT | 16 | ADAQ23876 ADC 2 channel data. To be used as input for the ADC CPAK IP. | | IP Data 2 OUT | 16 | ADAQ23876 ADC 2 channel data. To be used as input for the ADC CPAK IP. |
 | IP Data 3 OUT | 16 | ADAQ23876 ADC 3 channel data. To be used as input for the ADC CPAK IP. | | IP Data 3 OUT | 16 | ADAQ23876 ADC 3 channel data. To be used as input for the ADC CPAK IP. |
-CN0584 ​DAC Data 0 OUT | 16 | AD3552R_0 DAC 0 channel data. To be used as input into the AD3552R interface IP. | +CN0585 ​DAC Data 0 OUT | 16 | AD3552R_0 DAC 0 channel data. To be used as input into the AD3552R interface IP. | 
-CN0584 ​DAC Data 1 OUT | 16 | AD3552R_0 DAC 1 channel data. To be used as input into the AD3552R interface IP. | +CN0585 ​DAC Data 1 OUT | 16 | AD3552R_0 DAC 1 channel data. To be used as input into the AD3552R interface IP. | 
-CN0584 ​DAC Data 2 OUT | 16 | AD3552R_1 DAC 0 channel data. To be used as input into the AD3552R interface IP. | +CN0585 ​DAC Data 2 OUT | 16 | AD3552R_1 DAC 0 channel data. To be used as input into the AD3552R interface IP. | 
-CN0584 ​DAC Data 3 OUT | 16 | AD3552R_1 DAC 1 channel data. To be used as input into the AD3552R interface IP. |+CN0585 ​DAC Data 3 OUT | 16 | AD3552R_1 DAC 1 channel data. To be used as input into the AD3552R interface IP. |
 | IP Data Valid OUT     | 1 | Output signal that has to be logic '​1'​ for a clock cycle period when the data starts to be valid. ​ | | IP Data Valid OUT     | 1 | Output signal that has to be logic '​1'​ for a clock cycle period when the data starts to be valid. ​ |
 | IP Load Tx Data OUT   | 1 | Custom IP output signal used to notify the design that the IP is ready to receive new input data. The duration must be 1 clock cycle. | | IP Load Tx Data OUT   | 1 | Custom IP output signal used to notify the design that the IP is ready to receive new input data. The duration must be 1 clock cycle. |
Line 417: Line 415:
  
 {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0585:​rx_tx_configuration_lldk.png?​600 }} {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0585:​rx_tx_configuration_lldk.png?​600 }}
- 
  
  
resources/eval/user-guides/circuits-from-the-lab/cn0584.txt · Last modified: 25 Sep 2023 21:46 by Rukiye Guldali