Wiki

The most recent version of this page is a draft.DiffThis version (03 Oct 2023 15:46) was approved by Paul Blanchard.The Previously approved version (29 Sep 2023 16:41) is available.Diff

This is an old revision of the document!


CN0584 User Guide

CN0584 (Low Latency Development Kit) is a development platform consisting of two boards the EVAL-CN0585-FMCZ and the EVAL-CN0584-EBZ. EVAL-CN0585-FMCZ consists of 4 x 16-bit ADC channels and 4 x 16-bit DAC channels that are interfaced with an FPGA through the FMC Low Pin Count (LPC) Connector. Current revision of EVAL-CN0585-FMCZ is Rev B. EVAL-CN0584-EBZ is the application specific analog front end (AFE) board.CN0584 is connected to a Zedboard to build a development system setup like shown in Figure 7.

The Low Latency Development Kit (LLDK) provides a complete data acquisition and signal generation platform with on-board power rails, voltage monitoring, logic level translation, general purpose I/O, I2C, SPI, and a personality interface connector.

The key performance benefit of the LLDK system is the ability to perform a complete capture and conversion of precision analog input data in <70ns with the ADC module and generate a settled full-scale analog output in <200ns from initial data written to the DAC.

Figure 1. Low Latency Development Kit

Connections and Configurations

Figure 2. EVAL-CN0584-EBZ Board

Figure 3.Simplified Block Diagram of LLDK

ADC Inputs

There are four channels of differential input signals on EVAL-CN0584-EBZ.

Channel Positive Input Signal Negative Input Signal
Channel 0 J1 J2
Channel 1 J3 J4
Channel 2 J5 J6
Channel 3 J7 J8

Table 1. ADC Input Signal Connectors

ADC Input Range Configuration

LLDK has configurable input voltage ranges of ±10 V(Default), ±5 V, ±4.096 V, ±2.5 V, and ±1.5 V. The input range can be changed by modifying resistor placements on EVAL-CN0584-EBZ as described in Table 2.

Channel Input Voltage Range AFE Board Modification
Channel 0 ±10 V (default) Include R19A, R21A, R22A, R24A; DNI R18A, R20A, R23A, R25A
±5 V Include R18A, R20A, R23A, R25A; DNI R19A, R21A, R22A, R24A
±4.096 V Include R19A, R21A; DNI R18A, R20A, R22A, R23A, R24A, R25A
±2.5 V Include R18A, R20A; DNI R19A, R21A, R22A, R23A, R24A, R25A
±1.5 V Include R18A, R19A, R20A, R21A; DNI R22A, R23A, R24A, R25A
Channel 1 ±10 V (default) Include R19B, R21B, R22B, R24B; DNI R18B, R20B, R23B, R25B
±5 V Include R18B, R20B, R23B, R25B; DNI R19B, R21B, R22B, R24B
±4.096 V Include R19B, R21B; DNI R18B, R20B, R22B, R23B, R24B, R25B
±2.5 V Include R18B, R20B; DNI R19B, R21B, R22B, R23B, R24B, R25B
±1.5 V Include R18B, R19B, R20B, R21B; DNI R22B, R23B, R24B, R25B
Channel 2 ±10 V (default) Include R19C, R21C, R22C, R24C; DNI R18C, R20C, R23C, R25C
±5 V Include R18C, R20C, R23C, R25C; DNI R19C, R21C, R22C, R24C
±4.096 V Include R19C, R21C; DNI R18C, R20C, R22C, R23C, R24C, R25C
±2.5 V Include R18C, R20C; DNI R19C, R21C, R22C, R23C, R24C, R25C
±1.5 V Include R18C, R19C, R20C, R21C; DNI R22C, R23C, R24C, R25C
Channel 3 ±10 V (default) Include R19D, R21D, R22D, R24D; DNI R18D, R20D, R23D, R25D
±5 V Include R18D, R20D, R23D, R25D; DNI R19D, R21D, R22D, R24D
±4.096 V Include R19D, R21D; DNI R18D, R20D, R22D, R23D, R24D, R25D
±2.5 V Include R18D, R20D; DNI R19D, R21D, R22D, R23D, R24D, R25D
±1.5 V Include R18D, R19D, R20D, R21D; DNI R22D, R23D, R24D, R25D

Table 2. ADC Input Voltage Range Selection by Resistor Connections

DAC Outputs

LLDK can support multiple output voltage ranges which can be configured, such as 0 to 2.5 V, 0 V to 5 V, −5 V to +5 V, and −10 V to +10 V, and custom intermediate ranges with full 16-bit resolution. In order to change the output range, resistor placements on the AFE board must be modified and register settings must be applied to AD3552R on EVAL-CN0585-FMCZ as described in Table 4.

Channel Output Signal
A J9
B J10
C J11
D J12

Table 3. DAC Output Signal Connectors

Channel Output Span VZS (V) VFS (V) AFE Board Modification Register Setting
CH0+/- 10V (Default) -10.382 10.380 Include R9; DNI R10, R11 CH0_CH1_OUTPUT_RANGE = 0x100
+/- 5V -5.165 5.166 Include R11; DNI R9, R10 CH0_CH1_OUTPUT_RANGE = 0x011
10V -0.165 10.163 Include R11; DNI R9, R10 CH0_CH1_OUTPUT_RANGE = 0x010
5V -0.078 5.077 Include R10; DNI R9, R11 CH0_CH1_OUTPUT_RANGE = 0x001
2.5V -0.198 2.701 Include R10; DNI R9, R11 CH0_CH1_OUTPUT_RANGE = 0x000
CH1+/- 10V (Default) -10.382 10.380 Include R12; DNI R13, R14 CH0_CH1_OUTPUT_RANGE = 0x100
+/- 5V -5.165 5.166 Include R13; DNI R12, R14 CH0_CH1_OUTPUT_RANGE = 0x011
10V -0.165 10.163 Include R13; DNI R12, R14 CH0_CH1_OUTPUT_RANGE = 0x010
5V -0.078 5.077 Include R14; DNI R12, R13 CH0_CH1_OUTPUT_RANGE = 0x001
2.5V -0.198 2.701 Include R14; DNI R12, R13 CH0_CH1_OUTPUT_RANGE = 0x000
CH2+/- 10V (Default) -10.382 10.380 Include R15; DNI R16, R17 CH2_CH3_OUTPUT_RANGE = 0x100
+/- 5V -5.165 5.166 Include R16; DNI R15, R17 CH2_CH3_OUTPUT_RANGE = 0x011
10V -0.165 10.163 Include R16; DNI R15, R17 CH2_CH3_OUTPUT_RANGE = 0x010
5V -0.078 5.077 Include R17; DNI R15, R16 CH2_CH3_OUTPUT_RANGE = 0x001
2.5V -0.198 2.701 Include R17; DNI R15, R16 CH2_CH3_OUTPUT_RANGE = 0x000
CH3+/- 10V (Default) -10.382 10.380 Include R18; DNI R19, R20 CH2_CH3_OUTPUT_RANGE = 0x100
+/- 5V -5.165 5.166 Include R19; DNI R18, R20 CH2_CH3_OUTPUT_RANGE = 0x011
10V -0.165 10.163 Include R19; DNI R18, R20 CH2_CH3_OUTPUT_RANGE = 0x010
5V -0.078 5.077 Include R20; DNI R18, R19 CH2_CH3_OUTPUT_RANGE = 0x001
2.5V -0.198 2.701 Include R20; DNI R18, R19 CH2_CH3_OUTPUT_RANGE = 0x000

Table 4. DAC Output Voltage Range Selection by Resistor Connections and Register Settings

Voltage Reference

The default ADC reference configuration uses the internal 2.048 V, ±0.1% accurate, 20 ppm/°C max voltage reference. For more stringent use cases where the accuracy and temperature drift is an issue, an external LTC6655 2.048 V, ±0.025% accurate, 2 ppm/°C max voltage reference can be used.

The default DAC reference configuration uses the internal 2.5 V, ±0.3% accurate, 10 ppm/°C max voltage reference. For more stringent use cases where the accuracy and temperature drift is an issue, an external ADR4525 2.5 V, ±0.02% accurate, 2 ppm/°C max voltage reference can be used.

VREF Jumper Settings
ADC_VREF Short P5
DAC_VREF Short P4

Table 5. Voltage Reference Settings

Power Supply Considerations and Configuration

All power for CN0584 is provided by EVAL-CN0585-FMCZ through the AFE connector. CN0584 uses the +15 V and -15 V rails to provide the positive and negative supply voltages for the ADG5421F input protection switches. The +12 V and -12 V rails provide the positive and negative supply voltages for the ADA4898-1 ADC buffer amplifiers. The +3.3 V rail powers the EEPROM circuit. Table 6 provides more details on LLDK power rails:

Power Rail Description
+12 V LT3045-1 provides the 12V rail supplying up 280mA
-12 V LT3094 provides the -12V rail supplying up to -280mA
+15 V LTM8049 provides the +15V rail at 80% efficiency
-15 V LTM8049 provides the -15V rail at 80% efficiency
+3.3 V Fed through from the FPGA FMC connector to the AFE connector

Table 6. Power Rail Descriptions

System Setup Using a ZedBoard

CN0584 is fully supported using a ZedBoard.

Figure 4. EVAL-CN0585-FMCZ connected to EVAL-CN0584-EBZ

The following is a list of items needed for system setup:

  • Hardware
    • ZedBoard Rev D or later board
    • 12Vdc, 3A power supply
    • 16GB (or larger) Class 10 (or faster) micro-SD card (included in the box)
    • USB-C power source (included in the box)
    • Micro-USB to Type-A cable
    • Ethernet cable
    • User interface setup (choose one):
      • HDMI monitor, keyboard, and mouse plugged directly into the ZedBoard
      • Host Windows/Linux/Mac computer on the same network as the ZedBoard
  • Software
    • Host PC (Windows or Linux)
    • A UART terminal if need to access Linux system on the ZedBoard (Putty/Tera Term/Minicom, etc.), Baud rate 115200 (8N1)

Loading Image on SD Card

The box includes a pre-programmed SD card. You can skip the steps in this section and go to the Setting up the Hardware section if using this provided card.

To boot the ZedBoard and control the EVAL-CN0585-FMCZ, you will need to install ADI Kuiper Linux on an SD card. Complete instructions, including where to download the SD card image, how to write it to the SD card, and how to configure the system are provided on the Kuiper Linux page.

Configuring the SD Card

Follow the configuration procedure under Configuring the SD Card for FPGA Projects on the Kuiper Linux page. Copy the following files onto the boot directory to configure the SD card (download link sdcard_config_files.zip):

  • uImage file for Zynq
  • BOOT.BIN specific to your EVAL-CN0585-FMCZ + ZedBoard
  • setup_adc.sh file for setting up ADC
  • devicetree.dtb devicetree for Zynq specific to your EVAL-CN0585-FMCZ + ZedBoard.The device tree describes the following devices:
    1. one-bit-adc-dac – controls the MAX7301
    2. axi_pwm_gen – generates the CNV signal for analog-to-digital converters
    3. ref_clk – generates the sample clock for ADAQ23876 devices and the reference clock for AD3552R devices
    4. rx_dma – controls the DMA for RX path
    5. Ltc2387 – controls ADAQ23876 devices
    6. qspi0 – controls the SPI devices that are connected to the PL SPI IP
    7. dac0_tx_dma - controls the DMA for the first AD3552R device
    8. dac1_tx_dma - controls the DMA for the second AD3552R device
    9. axi_ad3552r_0 – controls the first AD3552R device
    10. axi_ad3552r_1 – controls the second AD3552R device
    11. I2c – controls devices that are connected to PL I2C IP (eeprom, eeprom2, ad7291_1)

Setting up the Hardware

You will need to:

  1. Get the ZedBoard.
  2. Insert the SD CARD into the SD Card Interface Connector (J12).
  3. Connect the EVAL-CN0585-FMCZ board into the ZedBoard FMC connector.
  4. Connect the EVAL-CN0584-EBZ board into the EVAL-CN0585-FMCZ.
  5. Connect micro USB to UART port (J14), and the other end to the host PC.
  6. Connect the ethernet cable to RJ45 ethernet connector (J11), and the other end to the host PC.
  7. Plug the Power Supply into the 12V Power ZedBoard input connector (J20) (DO NOT turn the device on).
  8. Plug USB-C power supply to EVAL-CN0585-FMCZ
  9. Set the jumpers as seen in Figure 5 zed_jumpers.jpgFigure 5. ZedBoard Jumper Settings
  10. Connect the DAC output connectors to the positive ADC input connectors as shown in Figure 6 using SMA cables. Terminate the negative ADC connectors with 50ohms terminators loopback_connection.jpg Figure 6. EVAL-CN0584-EBZ Loopback Connection on AFE
  11. Turn the ZedBoard on.
  12. Wait ~30 seconds for the “DONE” LED to turn blue. This is near the DISP1.The hardware set up is now complete.

Figure 7. Example System Setup

All the products described on this page include ESD (electrostatic discharge) sensitive devices. Electrostatic charges as high as 4000V readily accumulate on the human body or test equipment and can discharge without detection.

Although the boards feature ESD protection circuitry, permanent damage may occur on devices subjected to high-energy electrostatic discharges. Therefore, proper ESD precautions are recommended to avoid performance degradation or loss of functionality. This includes removing static charge on external equipment, cables, or antennas before connecting to the device.

Application Software (both locally and remotely on the FPGA)

The CN0584 can be interfaced with using IIO Oscilloscope, Python, or MATLAB to enable device configuration, capture of incoming samples from the ADCs, and generation of waveforms to be transmitted by the DACs.

Hardware Connection

Libiio is a library used for interfacing with IIO devices and must be installed on your computer to interface with the hardware.

Download and Install the latest Libiio package on your machine.

To connect to your device, the IIO Osciloscope software must be able to create a context. The context creation in the software depends on the backend used to connect to the device as well as the platform where the EVAL-CN0585-FMCZ is attached. The ZedBoard running ADI Kuiper Linux is currently the only platform supported for the CN0585.

The user needs to supply a URI (Uniform Resource Identifier) which will be used in the context creation. To get the URI, use the command iio_info in the terminal. The iio_info command is a part of the libIIO package that reports all IIO attributes.Upon installation, simply enter the command on the terminal command line to access it.

For FPGA(ZedBoard) Direct Local Access:

iio_info

For Windows machine connected to an FPGA(ZedBoard):

iio_info -u ip:<ip address of your ip>

Example:

  • If your ZedBoard has the IP address 169.254.92.202, you have to use iio_info -u ip::169.254.92.202 as your URI
Do note that the Windows machine and the FPGA board should be connected to the same network for the machine to detect the device.

IIO Oscilloscope

IIO Oscilloscope is a cross platform GUI application which can interface with different evaluation boards from within a Linux system.

Make sure to download/update to the latest version of IIO-Oscilloscope found on this linkhttps://github.com/analogdevicesinc/iio-oscilloscope/releases
  • 1- Once done with the installation or an update of the latest IIO-Oscilloscope, open the application. The user needs to supply a URI which will be used in the context creation of the IIO Oscilloscope. If there's only one platform is connected, the IIO Oscilloscope will find URI automatically; If more than one platforms are connected, the user needs to supply the specific URI. The instructions to obtain the URI can be found in the previous section.
  • 2- Press refresh to display available IIO Devices and press connect.

Figure 8. IIO Oscilloscope Connection

  • 3- After the board is connected, select the one-bit-adc-dac-device, which is the controller for the MAX7301ATL+ I/O Expander. Then configure pins values of output voltages 0 through 9, by setting the raw value to 1 . Press Write to confirm.

Figure 9. MAX7301ATL Output Channels Configuration

one-bit-adc-dac device channel Schematic PIN
Voltage0 GPIO0_VIO
Voltage1 GPIO1_VIO
Voltage2 GPIO2_VIO
Voltage3 GPIO3_VIO
Voltage4 GPIO6_VIO
Voltage5 GPIO7_VIO
Voltage6 PAD_ADC0
Voltage7 PAD_ADC1
Voltage8 PAD_ADC2
Voltage9 PAD_ADC3

Table 7. Voltage Configuration for GPIO Pins

  • 4- Select the desired input source for both AD3552R devices axi-ad3552r-0 and axi-ad3552r-1 as dma_input. Figure 10. AD3552R Input Source Selection in IIO Oscilloscope
Even if the input source is set to adc_input or ramp_input the steps regarding the DAC Data Manager tab have to be followed.
  • 5- Select the desired output range for both AD3552R devices. Figure 11. AD3552R Output Range Selection in IIO Oscilloscope
Make sure you don't try to read/write the output_range attribute when the stream_status is in start_stream or start_stream_synced.
  • 6- From the DAC Data Manager Window select the output channels of the DAC and enable the cyclic buffer for each DAC.
  • 7- Load an example file (.mat, .txt, etc) from the IIO Oscilloscope installation directory, under Program Files/IIO Oscilloscope/lib/osc/waveforms folder.
If the source is set as dma_input and the data from all 4 channels needs to be synchronized make sure that you press the load button for the axi-ad3552r-1 device first then for axi-ad3552r-0.

dac_data_management_cn0585.jpg Figure 12. DAC Data Manager with Example Waves on 4 Channels

  • 8- Click on the load button.
If the source is set as dma_input and the data from all 4 channels needs to be synchronized make sure that you write the start_stream_synced for the axi-ad3552r-1 device first then for axi-ad3552r-0.
  • 9- From the Debug window, select the stream_status IIO Attribute and start the stream (start_stream_synced means that all 4 channels are updated at the same time and the data streaming process waits for both DACs to be started).

stream_status_iio.jpgFigure 13. DAC Stream Status Selection

If the source is set as dma_input and the data from all 4 channels needs to be synchronized make sure that you write the start_stream_synced for the axi-ad3552r-1 device first then for axi-ad3552r-0.
  • 10- After the stream_status has been written and 4 channels are enabled, hit play button. Then data capture window can be seen like in Figure 14. captured_loopback_signal_cn0585.jpgFigure 14. Captured Loopback Signal
Note that there is a phase delay between voltage0/voltage2 and voltage1/voltage3 because the DAC device channels are updated consecutively See the DAC UPDATE MODES section in AD3552R
If you intend to stop the stream transmission and start it again synchronized set the stream_status IIO Attribute to stop_stream for axi-ad3552r-1 device first then for the axi-ad3552r-0 device.

PyADI-IIO

The CN0584 can be interfaced to Python using the PyADI-IIO. PyADI-IIO is a Python abstraction module to simplify interaction with IIO drivers on ADI hardware. This module provides device-specific APIs built on top of the current libIIO Python bindings. These interfaces try to match the driver naming as much as possible without the need to understand the complexities of libIIO and IIO.

Follow the step-by-step procedure on how to install, configure, and set up PyADI-IIO and install the necessary packages/modules needed by referring to PyADI-IIO.

Running the example

Github link for the Python sample script: CN0585 Python Example

After installing and configuring PYADI-IIO on your machine, you are now ready to run Python script examples. To follow this example, run the cn0585_fmcz_example.py found in the examples folder.

D:\pyadi-iio>export PYTHONPATH=D:/pyadi-iio/ 
D:\pyadi-iio>python examples/cn0585_fmcz_example.py ip:your_board_ip

Press enter and lines below will be observed:

$ python examples/cn0585_fmcz_example.py
uri: ip:your_board_ip
############# EEPROM INFORMATION ############
read 256 bytes from /sys/devices/soc0/fpga-axi@0/41620000.i2c/i2c-1/1-0050/eeprom
Date of Man     : Fri Jan 20 08:11:00 2023
Manufacturer    : Analog Devices
Product Name    : LLDK-LTC2387-AD3552R
Serial Number   : 56864654
Part Number     : 1234
FRU File ID     : 12131321
PCB Rev         : VB
PCB ID          : HIL
BOM Rev         : VC
Uses LVDS       : Y

#############################################
GPIO4_VIO state is: 0
GPIO5_VIO state is: 0
Voltage monitor values:
Channel :  temp0 :  49.25 Deg. C
Channel :  voltage0 :  2.26745605283 V
Channel :  voltage1 :  0.6274414057359999 V
Channel :  voltage2 :  2.061157224874 V
Channel :  voltage3 :  0.7531738275079999 V
Channel :  voltage4 :  2.092285154536 V
Channel :  voltage5 :  2.084960935792 V
Channel :  voltage6 :  2.2534179669039998 V
Channel :  voltage7 :  1.80969238133 V
AXI4-Lite 0x108 register value: 0x2
AXI4-Lite 0x10c register value: 0xB
Sample data min: 0
Sample data max: 65535
input_source:dac0: adc_input
input_source:dac1: adc_input
Maximum measured voltage 0 : 10.115187500000001
Maximum measured voltage 1 : 0.00103125
Maximum measured voltage 2 : 0.00034375000000000003
Maximum measured voltage 3 : 0.00103125
Minimum measured voltage 0: 10.107625
Minimum measured voltage 1: -0.00034375000000000003  
Minimum measured voltage 2: -0.00103125
Minimum measured voltage 3: -0.00034375000000000003

The following window will pop up:

python_plot.jpgFigure 15: ADC Captured Data Python Plot

If you plan to transmit multiple cycles of synchronous stream, make sure the script starts/stops axi-ad3552r-1 first, then axi-ad3552r-0.

Device Control and Data Streaming

Remote data streaming to and from hardware is made available through system object interfaces, which are unique for each component or platform. The hardware interfacing system objects provide a class to both configure a given platform and move data back and forth from the device. After running the CN0585StreamingTest.m example as described in Steps for MATLAB Configuration of CN0585, the window in Figure 16 will pop up:

matlab_plot.jpgFigure 16. ADC Captured Data Matlab Plot

If you plan to transmit multiple cycles of synchronous stream, make sure to start/stop axi-ad3552r-1 first, then axi-ad3552r-0.

The ZedBoard that drives CN0585 is configured with a HDL reference design which is an embedded system built around a processor core either ARM, NIOS-II, or Microblaze. A functional block diagram of the system is shown in Figure 17.

Figure 17. HDL Reference Design

The device digital interface is handled by specific device cores axi_ad35552r for the DAC path and axi_ltc2387 for the ADC path. The cores are programmable through an AXI-lite interface. HDL IP(HDL_DUT) code to be integrated in this reference design is generated using High Speed Converter Toolbox. (https://github.com/analogdevicesinc/HighSpeedConverterToolbox/). High Speed Converter Toolbox supports the IP Core generation flow from MathWorks which allows for automated integration of DSP into HDL reference designs from Analog Devices. The workflow for generating HDL_DUT codes takes Simulink subsystems, runs HDL-Coder to generate source Verilog, and then integrates that into a larger reference design. HDL_DUT Code Generation Workflow is described in configuring_lldk.pdf. HDL_DUT with Configuration Registers (Accessed over AXI-Lite Interface) Code Generation Workflow for Transmit Configuration is described in configuring_lldk_axi_lite.pdf

Schematic, PCB Layout, Bill of Materials

EVAL-CN0584-EBZ Design & Integration Files

  • Schematics
  • PCB Layout
  • Bill of Materials
  • Allegro Project

Reference Demos & Software

/srv/wiki.analog.com/data/pages/resources/eval/user-guides/circuits-from-the-lab/cn0584.txt · Last modified: 05 Dec 2023 17:23 by Xiaomeng Gao