Both sides previous revisionPrevious revision | |
resources:eval:user-guides:circuits-from-the-lab:cn0582 [18 Nov 2022 09:29] – Nov18_4-29 Michelle Claire So | resources:eval:user-guides:circuits-from-the-lab:cn0582 [23 Nov 2022 01:55] (current) – Nov23_8-55 Michelle Claire So |
---|
====== USB 3.0 Based Multi-Channel Test Platform for Vibration Sensors User Guide ====== | ====== USB 3.0 Quad-Channel IEPE Vibration Sensor Measurement System ====== |
| |
===== General Description ===== | ===== General Description ===== |
CN0582 or the USB 3.0 Based Multi-Channel Test Platform for Vibration Sensors is a system board capable of reading data from analog (IEPE) accelerometers. The analog IEPE inputs also contain current source switches to accommodate sensors that might need external power and individual channel offset voltage setting.\\ | CN0582 or the USB 3.0 Quad-Channel IEPE Vibration Sensor Measurement System is a system board capable of reading data from analog (IEPE) accelerometers. The analog IEPE inputs also contain current source switches to accommodate sensors that might need external power and individual channel offset voltage setting.\\ |
| |
Aside from IEPE sensor measurements, the board is also an arbitrary sine wave generator providing stimulus to an external vibration shaker and a multi-channel data acquisition system. | Aside from IEPE sensor measurements, the board is also an arbitrary sine wave generator providing stimulus to an external vibration shaker and a multi-channel data acquisition system. |
---- | ---- |
===== Requirements ===== | ===== Requirements ===== |
The USB 3.0 Based Multi-Channel Test Platform is a complete system from Hardware, Firmware, to Software for performing basic Data acquisition (DAQ) functions and vibration tests. \\ \\ The following sections will detail the necessary steps and conditions needed to fully operate the system. \\ | The USB 3.0 Quad-Channel IEPE Vibration Sensor Measurement System is a complete system from Hardware, Firmware, to Software for performing basic Data acquisition (DAQ) functions and vibration tests. \\ \\ The following sections will detail the necessary steps and conditions needed to fully operate the system. \\ |
| |
**<fc #6495ed>Firmware</fc>** \\ | **<fc #6495ed>Firmware</fc>** \\ |
Once the USB 3.0 Based Multi-Channel Test Platform software is installed via the given installer (Refer to the Installation Guide section), the compatible firmware is located within the same folder as the GUI executable file. \\ | Once the USB 3.0 Quad-Channel IEPE Vibration Sensor Measurement System is installed via the given installer (Refer to the Installation Guide section), the compatible firmware is located within the same folder as the GUI executable file. \\ |
| |
At startup, the GUI uploads the firmware to the board for easier use. Do not remove the firmware (.img file) in the folder to avoid errors. {{ :resources:eval:user-guides:multi-channel-vibration-test-platform:0582_firmware_image.png?nolink&600 |}} \\ Should there be any updates necessary, uninstall the GUI and corresponding files using the uninstaller (C:\Analog Devices\USB3.0 Based Multi-Channel Test Platform for Vibration Sensor\Uninstall.exe). An updated installer containing the updated firmware and other files will be uploaded for download. \\ | At startup, the GUI uploads the firmware to the board for easier use. Do not remove the firmware (.img file) in the folder to avoid errors. {{ :resources:eval:user-guides:multi-channel-vibration-test-platform:0582_firmware_image.png?nolink&600 |}} \\ Should there be any updates necessary, uninstall the GUI and corresponding files using the uninstaller (C:\Analog Devices\USB3.0 Based Multi-Channel Test Platform for Vibration Sensor\Uninstall.exe). An updated installer containing the updated firmware and other files will be uploaded for download. \\ |
</WRAP> | </WRAP> |
\\ | \\ |
**<fc #6495ed>GUI Installer</fc>** \\ This will setup the dependencies folder which will also contain the USB 3.0 Based Multi-Channel Test Platform GUI executable file. | **<fc #6495ed>GUI Installer</fc>** \\ This will setup the dependencies folder which will also contain the USB 3.0 Quad-Channel IEPE Vibration Sensor Measurement System GUI executable file. |
| |
**<fc #6495ed>Driver Installer</fc>** \\ Running the driver installer is necessary to fully setup the necessary drivers and make the board recognizable by the software. \\ {{ :resources:eval:user-guides:multi-channel-vibration-test-platform:fx3.png?nolink&600 |}} | **<fc #6495ed>Driver Installer</fc>** \\ Running the driver installer is necessary to fully setup the necessary drivers and make the board recognizable by the software. \\ {{ :resources:eval:user-guides:multi-channel-vibration-test-platform:fx3.png?nolink&600 |}} |
* The Shaker must be initially off before setting and running the necessary parameters. \\ \\ | * The Shaker must be initially off before setting and running the necessary parameters. \\ \\ |
| |
4. Toggle the current source (for IEPE accelerometer), gain, coupling, and sensor dc bias settings as needed. {{ :resources:eval:user-guides:multi-channel-vibration-test-platform:htu_daq.png?nolink&3000 |}} | 4. Toggle the current source (for IEPE accelerometer), gain, coupling, and sensor dc bias settings as needed. {{ :resources:eval:user-guides:multi-channel-vibration-test-platform:htu_vibration_test.png?nolink&3000 |}} <note important> Vibration Testing Window Settings </note> |
<note important>DAQ Window Settings</note> {{ :resources:eval:user-guides:multi-channel-vibration-test-platform:htu_vibration_test.png?nolink&3000 |}} <note important> Vibration Window Settings </note> | |
| |
5. On the channel selector section, enable the channel where the other Analog Input source is connected. \\ | 5. On the channel selector section, enable the channel where the other Analog Input source is connected. \\ |
| |
6. Click set when the parameters have been chosen, then press Start to launch the test. | 6. Click set when the parameters have been chosen, then press Start to launch the test. |