This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | Next revision Both sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0575 [18 May 2023 21:12] Brandon Bushey [General Description] |
resources:eval:user-guides:circuits-from-the-lab:cn0575 [18 May 2023 23:35] Mark Thoren Add CN0575-specific example |
||
---|---|---|---|
Line 257: | Line 257: | ||
\\ | \\ | ||
---- | ---- | ||
+ | ==== More Complete Example with Digital I/O ==== | ||
+ | A more complete example that blinks the onboard LED and reads the pushbutton is also provided. Note that this script can be run either directly on the Raspberry Pi, or from a remote host computer. | ||
+ | \\ | ||
+ | From the Raspberry Pi command line, run: | ||
+ | <code>.../pyadi-iio/examples $ sudo python cn0575_example.py</code> | ||
+ | Or from PowerShell on a Windows remote host, run: | ||
+ | <code>...\pyadi-iio\examples> python .\cn0575_example.py</code> | ||
+ | The script will attempt to automatically locate the CN0575 over the network connection. The CN0575's IIO context URI can also be passed to the script explicitly, where **www.xxx.yyy.zzz** is the board's IP address: | ||
+ | <code>C:\temp\pyadi-iio\examples> python .\cn0575_example.py ip:www.xxx.yyy.zzz</code> | ||
+ | Typical output is shown below: | ||
+ | \\ | ||
+ | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0575:cn0575_example_screenshot.png?nolink&500 |}} | ||
+ | \\ | ||
+ | ---- | ||
===== Schematic, PCB Layout, Bill of Materials ===== | ===== Schematic, PCB Layout, Bill of Materials ===== | ||