This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0552 [27 Sep 2022 03:54] – add hw connectors section + grammar edits Trisha Cabildo | resources:eval:user-guides:circuits-from-the-lab:cn0552 [22 Nov 2023 09:46] (current) – fix broken link Darius B | ||
---|---|---|---|
Line 65: | Line 65: | ||
| GND | 2 | | | GND | 2 | | ||
| IOVDD | 1 | | | IOVDD | 1 | | ||
+ | |||
+ | ==== Solder Jumpers ==== | ||
+ | Eight solder jumpers are available at the bottom of the board, if you want to change the operating modes. | ||
+ | |||
+ | {{: | ||
+ | ^ Description and default connection | ||
+ | | ADC SDA connection (pull-up SDA to VDD) | P1 | Shorted | ||
+ | | ADC SCL connection (pull-up SCL to VDD) | P7 | Shorted | ||
+ | | Extended Excitation Enable (connect A1 OUT to P8 pin 3) | P14 | Shorted | ||
+ | | ADC REFIN(-) connection (connect GND and P8 pin 5) | P3 | Open | | ||
+ | | ADC REFIN(+) connection (connect GND and P8 pin 4) | P9 | Open | | ||
+ | | ADC CIN1(-) connection (connect GND to P8 pin 7) | P4 | Open | | ||
+ | | ADC CIN1(+) connection (connect GND to P8 pin 8) | P10 | Open | | ||
+ | | ADC CIN2(-) connection (connect GND to P13 pin 7) | P5 | Open | | ||
+ | | ADC CIN1(+) connection (connect GND to P13 pin 8) | P11 | Open | | ||
+ | | ADC VIN(-) connection (connect GND to P13 pin 4) | P6 | Open | | ||
+ | | ADC VIN(+) connection (connect GND to P13 pin 5) | P12 | Open | | ||
+ | |||
+ | ==== Test Points ==== | ||
+ | Also, four test points are available to probe the I2C interface. | ||
===== Device Driver Support ===== | ===== Device Driver Support ===== | ||
Line 114: | Line 134: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
Prebuilt CN0552 Hex File | Prebuilt CN0552 Hex File | ||
- | * [[repo> | + | * [[repo> |
Complete CN0552 Source Files | Complete CN0552 Source Files | ||
Line 154: | Line 174: | ||
* **Software** | * **Software** | ||
- | * [[: | + | * [[: |
==== Loading Image on SD Card ==== | ==== Loading Image on SD Card ==== | ||
- | In order to control the **EVAL-CN0552-PMDZ** from the Raspberry Pi, you will need to install ADI Kuiper Linux on an SD card. Complete instructions, | + | In order to control the **EVAL-CN0552-PMDZ** from the Raspberry Pi, you will need to install ADI Kuiper Linux on an SD card. Complete instructions, |
+ | \\ | ||
\\ | \\ | ||
Write the image and follow the system configuration procedure. | Write the image and follow the system configuration procedure. | ||
==== Configuring the SD Card ==== | ==== Configuring the SD Card ==== | ||
- | Follow the Hardware Configuration procedure under **Preparing the Image: Raspberry Pi** in the [[: | + | Follow the Hardware Configuration procedure under **Preparing the Image: Raspberry Pi** in the [[: |
< | < | ||
Line 301: | Line 322: | ||
* [[repo> | * [[repo> | ||
* [[repo> | * [[repo> | ||
- | * [[: | + | * [[: |
| | ||
=====Registration===== | =====Registration===== |