This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:circuits-from-the-lab:cn0552 [09 Mar 2022 21:06] Robin Getz fix link |
resources:eval:user-guides:circuits-from-the-lab:cn0552 [10 Mar 2022 15:48] (current) Brandon Bushey [Demo Requirements] updating to use PMD-RPI-INTZ |
||
---|---|---|---|
Line 136: | Line 136: | ||
* **Hardware** | * **Hardware** | ||
* [[ADI>CN0552|EVAL-CN0552-PMDZ]] | * [[ADI>CN0552|EVAL-CN0552-PMDZ]] | ||
- | * [[:resources:eval:user-guides:circuits-from-the-lab:pmd-rpi-intz|PMOD to Raspberry Pi Adapter (PMD-RPI-INTZ)]] | + | * [[ADI>PMD-RPI-INTZ|PMOD to Raspberry Pi Adapter (PMD-RPI-INTZ)]] |
* Raspberry PI Zero, Zero W, 3B+, or 4 | * Raspberry PI Zero, Zero W, 3B+, or 4 | ||
* 16GB (or larger) Class 10 (or faster) micro-SD card | * 16GB (or larger) Class 10 (or faster) micro-SD card | ||
* 5Vdc, 2.5A power supply with micro USB connector (USB-C power supply for Raspberry Pi 4) | * 5Vdc, 2.5A power supply with micro USB connector (USB-C power supply for Raspberry Pi 4) | ||
- | * Electrical connection hardware (choose one): | ||
- | * 12x 15cm socket-to-socket jumpers such as [[https://schmartboard.com/wire-jumpers/female-jumpers/5-inch/|these from Schmartboard]] | ||
- | * [[https://reference.digilentinc.com/reference/add-ons/pmod-hat/start|DesignSpark HAT to Pmod Adapter]] | ||
* User interface setup (choose one): | * User interface setup (choose one): | ||
* HDMI monitor, keyboard, mouse plugged directly into Raspberry Pi | * HDMI monitor, keyboard, mouse plugged directly into Raspberry Pi |