This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0548 [28 Jan 2022 13:30] – [Flashing the Firmware/Program] Harvey John De Chavez | resources:eval:user-guides:circuits-from-the-lab:cn0548 [04 Feb 2022 08:10] (current) – [Flashing the Firmware/Program] Harvey John De Chavez | ||
---|---|---|---|
Line 106: | Line 106: | ||
Prebuilt CN0548 Hex File | Prebuilt CN0548 Hex File | ||
- | * {{ : | + | * [[repo> |
- | * {{ : | + | * [[repo> |
Complete CN0548 Source Files | Complete CN0548 Source Files | ||
* [[repo> | * [[repo> | ||
Line 126: | Line 126: | ||
\\ \\ | \\ \\ | ||
+ | ---- | ||
====PyADI-IIO ==== | ====PyADI-IIO ==== | ||
PyADI-IIO is a python abstraction module for ADI hardware with IIO drivers to make them easier to use. This module provides device-specific APIs built on top of the current libIIO python bindings. These interfaces try to match the driver naming as much as possible without the need to understand the complexities of libIIO and IIO. | PyADI-IIO is a python abstraction module for ADI hardware with IIO drivers to make them easier to use. This module provides device-specific APIs built on top of the current libIIO python bindings. These interfaces try to match the driver naming as much as possible without the need to understand the complexities of libIIO and IIO. |