This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0548 [28 Jan 2022 13:07] – [Configuring the Absolute Input Voltage Range] Harvey John De Chavez | resources:eval:user-guides:circuits-from-the-lab:cn0548 [04 Feb 2022 08:10] (current) – [Flashing the Firmware/Program] Harvey John De Chavez | ||
---|---|---|---|
Line 58: | Line 58: | ||
\\ | \\ | ||
\\ | \\ | ||
+ | \\ \\ | ||
==== Chip Select ==== | ==== Chip Select ==== | ||
As mentioned in the Features section earlier, the CN0548 has a remappable Chip Select feature allowing the board to be stacked with other shields. By default, jumper P15 is shunted but this can be modified accordingly depending on the shields stacked and the user's application. \\ | As mentioned in the Features section earlier, the CN0548 has a remappable Chip Select feature allowing the board to be stacked with other shields. By default, jumper P15 is shunted but this can be modified accordingly depending on the shields stacked and the user's application. \\ | ||
Line 105: | Line 106: | ||
Prebuilt CN0548 Hex File | Prebuilt CN0548 Hex File | ||
- | * {{ : | + | * [[repo> |
- | * {{ : | + | * [[repo> |
Complete CN0548 Source Files | Complete CN0548 Source Files | ||
* [[repo> | * [[repo> | ||
Line 125: | Line 126: | ||
\\ \\ | \\ \\ | ||
- | \\ | + | ---- |
====PyADI-IIO ==== | ====PyADI-IIO ==== | ||
+ | PyADI-IIO is a python abstraction module for ADI hardware with IIO drivers to make them easier to use. This module provides device-specific APIs built on top of the current libIIO python bindings. These interfaces try to match the driver naming as much as possible without the need to understand the complexities of libIIO and IIO. | ||
- | [[/ | + | <note tip> |
- | + | Not yet familiar | |
- | ===Installing and Setting up the PyADI-IIO | + | </ |
- | - There are minimal variations in installing PyADI-IIO depending on your operating system. | + | |
- | - Upon performing the OS-specific steps, we will also be needing the matplotlib package for the plotting of data: < | + | |
- | < | + | |
\\ | \\ | ||