Next revision Both sides next revision
resources:eval:user-guides:circuits-from-the-lab:cn0548 [22 Sep 2021 03:35]
erbe reyta [Simplified Block Diagram]
resources:eval:user-guides:circuits-from-the-lab:cn0548 [29 Sep 2021 05:49]
erbe reyta [Simplified Block Diagram]
Line 17: Line 17:
  
  
- ​2. Follow the figure below for the position of shunt jumpers for headers P1, P3, P10, P8, P9, and P11. Make sure that is set at 16V max input for the voltage sensing, follow jumper settings stated in the table below encircled in red for 16V maximum input.+  
 +1. Place the shunt jumpers connected to P15 as the default position for the Chip Select. 
 +{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0548:​chip_select_default_settings.png?​400 |}} 
 +2. Follow the figure below for the position of shunt jumpers for headers P1, P3, P10, P8, P9, and P11. Make sure that is set at 16V max input for the voltage sensing, follow jumper settings stated in the table below encircled in red for 16V maximum input.
  
 {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0548:​limit_table_vsense.png?​600|}} {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0548:​limit_table_vsense.png?​600|}}
resources/eval/user-guides/circuits-from-the-lab/cn0548.txt · Last modified: 24 Nov 2021 03:14 by Harvey John De Chavez