Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
resources:eval:user-guides:circuits-from-the-lab:cn0545 [19 Jul 2022 09:09] – John Carlo Cillion | resources:eval:user-guides:circuits-from-the-lab:cn0545 [22 Feb 2023 02:44] – [Overview] Rod Joervie Adante |
---|
This user guide will discuss how to operate the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD7124-4?doc=cn0383.pdf/|EVAL-AD7124-4SDZ]]/[[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD7124-8?doc=cn0383.pdf/|EVAL-AD7124-8SDZ]] (CN-0545 Evaluation Hardware), the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/SDP-B.html|EVAL-SDP-CB1Z]] (SDP-B) and the [[ftp://ftp.analog.com/pub/evalcd/AD7124 |AD7124_EVAL+ Software]]. A complete design support package for the CN-0545 evaluation material containing schematics, layouts (native and Gerber), and bill-of-materials can be found at: [[adi>CN0545-DesignSupport|CN0545-DesignSupport]]. | This user guide will discuss how to operate the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD7124-4?doc=cn0383.pdf/|EVAL-AD7124-4SDZ]]/[[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD7124-8?doc=cn0383.pdf/|EVAL-AD7124-8SDZ]] (CN-0545 Evaluation Hardware), the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/SDP-B.html|EVAL-SDP-CB1Z]] (SDP-B) and the [[ftp://ftp.analog.com/pub/evalcd/AD7124 |AD7124_EVAL+ Software]]. A complete design support package for the CN-0545 evaluation material containing schematics, layouts (native and Gerber), and bill-of-materials can be found at: [[adi>CN0545-DesignSupport|CN0545-DesignSupport]]. |
| |
{{ :resources:eval:user-guides:circuits-from-the-lab:ad7124-singlethermistor.png |}} | {{ :resources:eval:user-guides:ad7124:ad7124-singlethermistor.png?nolink&600 |}} |
| |
===== Required Equipment ===== | ===== Required Equipment ===== |
* Power the board with a 7 V or 9 V power source connected to J5. | * Power the board with a 7 V or 9 V power source connected to J5. |
* Connect the Thermistor and precision reference resistor. See figure below. | * Connect the Thermistor and precision reference resistor. See figure below. |
| * For Thermistor measurements, ensure that the following jumpers and links are properly connected. |
| * LK3 - Jumper from REFIN1- to AVSS, this jumper should be inserted. |
| * LK4 - This jumper is used to apply an external 2.5V or internal 2.5V to REFIN1+, this jumper should be inserted to B. |
* Connect the SDP board to the PC via the USB cable. | * Connect the SDP board to the PC via the USB cable. |
| |
{{ :resources:eval:user-guides:circuits-from-the-lab:thermistor_demo_eval.png?600 |}} | {{ :resources:eval:user-guides:circuits-from-the-lab:thermistor_demo_eval.png?600 |}} |
==== Demo Mode and ADC Software Configurations ==== | ==== Demo Mode and ADC Software Configurations ==== |
To configure the [[adi>en/products/ad7124-4.html|AD7124-4]]/[[adi>en/products/ad7124-8.html|AD7124-8]] for Thermistor measurement, click the **Thermistor demo mode button** (see Figure above). Clicking the demo mode button configures the ADC software for Thermistor configurations. Additional instructions is provided regarding the links when the '?' button is clicked. | To configure the [[adi>en/products/ad7124-4.html|AD7124-4]]/[[adi>en/products/ad7124-8.html|AD7124-8]] for Thermistor measurement, click the **Thermistor demo mode button** (see Figure above). Clicking the demo mode button configures the ADC software for Thermistor configurations. Additional instructions are provided regarding the thermistor configuration when the {{:resources:eval:user-guides:circuits-from-the-lab:qq.png?30|}} button is clicked. |
| |
=== Thermistor demo mode === | === Thermistor demo mode === |