Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
Next revision Both sides next revision
resources:eval:user-guides:circuits-from-the-lab:cn0545 [11 Feb 2021 17:32]
Ioana Chelaru
resources:eval:user-guides:circuits-from-the-lab:cn0545 [05 Sep 2022 08:22]
John Carlo Cillion
Line 45: Line 45:
   * Power the board with a 7 V or 9 V power source connected to J5.   * Power the board with a 7 V or 9 V power source connected to J5.
   * Connect the Thermistor and precision reference resistor. See figure below. ​   * Connect the Thermistor and precision reference resistor. See figure below. ​
 +  * For Thermistor measurements,​ ensure that the following jumpers and links are properly connected.
 +      * LK3 - Jumper from REFIN1- to AVSS, this jumper should be inserted.
 +      * LK4 - This jumper is used to apply an external 2.5V or internal 2.5V to REFIN1+, this jumper should be inserted to B.
   * Connect the SDP board to the PC via the USB cable.   * Connect the SDP board to the PC via the USB cable.
  
Line 64: Line 67:
 {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​thermistor_demo_eval.png?​600 |}} {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​thermistor_demo_eval.png?​600 |}}
 ==== Demo Mode and ADC Software Configurations ==== ==== Demo Mode and ADC Software Configurations ====
-To configure the [[adi>​en/​products/​ad7124-4.html|AD7124-4]]/​[[adi>​en/​products/​ad7124-8.html|AD7124-8]] for Thermistor measurement,​ click the **Thermistor demo mode button** (see Figure above). Clicking the demo mode button configures the ADC software for Thermistor configurations. ​+To configure the [[adi>​en/​products/​ad7124-4.html|AD7124-4]]/​[[adi>​en/​products/​ad7124-8.html|AD7124-8]] for Thermistor measurement,​ click the **Thermistor demo mode button** (see Figure above). Clicking the demo mode button configures the ADC software for Thermistor configurations. Additional instructions are provided regarding the thermistor configuration when the {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​qq.png?​30|}} button is clicked.
  
 === Thermistor demo mode === === Thermistor demo mode ===
resources/eval/user-guides/circuits-from-the-lab/cn0545.txt · Last modified: 22 Feb 2023 03:13 by Rod Joervie Adante