Wiki

This version is outdated by a newer approved version.DiffThis version (14 Jan 2021 05:20) was approved by Robin Getz.The Previously approved version (30 Sep 2020 14:35) is available.Diff

This is an old revision of the document!


CN0540 HDL Reference Design

Overview

The HDL reference design for the CN0540 provides all the interfaces that are necessary to interact with the devices on the 24-bit data acquisition system designed for IEPE sensors.

The design have a SPI Engine instance to control and acquire data from the AD7768-1 24-bit precisions ADC, providing support to capture continuous samples at maximum sampling rate. Currently the design support FPGA carriers from both Intel and Xilinx.

Used devices

Evaluation board

Supported FPGA carrier

HDL Design Description

The design is built upon ADI's generic HDL reference design framework. In the ADI Reference Designs HDL User Guide can be found an in-depth presentation and instructions about the HDL design framework in general.

The reference design uses the standard SPI Engine Framework to interface the AD7768-1 ADC. The SPI offload module, which can be used to capture continuous data stream at maximum data rate, is triggered by the DRDY (data ready) signal of the device.

In order to build the HDL design the user has to go through the following steps:

  1. Confirm that you have the right tools (see Release notes)
  2. Clone the HDL GitHub repository (see https://wiki.analog.com/resources/fpga/docs/git)

HDL Downloads

Software sources

resources/eval/user-guides/circuits-from-the-lab/cn0540/hdl.1610597529.txt.gz · Last modified: 14 Jan 2021 05:12 by Robin Getz