This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0536 [20 Jan 2021 14:26] – Jardine Peñaflor | resources:eval:user-guides:circuits-from-the-lab:cn0536 [13 Jan 2022 14:59] (current) – [More Information and Useful Links] Brandon Bushey | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== EVAL-CN0536-ARDZ Shield Overview | + | ===== EVAL-CN0536-ARDZ Shield Overview ===== |
- | Geiger counters are most commonly used by people | + | Geiger counters are one of the most commonly used tools to measure radiation levels. This is a popular sensor in other countries like Japan where power is mainly generated from nuclear plants. This type of sensor is generally |
- | EVAL-CN0536-ARDZ is a low-power Geiger counter radiation detector in an Arduino shield form factor that can run on 3V to 5V system supply. It has a low cost, high voltage generation power supply that is robust and adjustable voltage output from 280V to 500V output. One of the key major part of the circuit in figure 1 is to generate high voltage output using Analog Devices precision programmable oscillator that is versatile, compact and easy to use LTC6906 that can be set to run oscillate from 10khz to 1Mhz using single user defined resistor value. This reference circuit design is compatible with most of the Geiger-Muller tube sensors available in the market today with a voltage rating between 280V to 500V. | + | |
- | To set and regulate the high voltage output supply and capture Geiger-Muller tube distinct pulses , the circuit shown in figure 1 has Analog devices LTC1540, a nano power comparator with built in voltage reference to precisely set the user required voltage output and LTC1441 ultralow power dual comparator to translate Geiger pulse to logic level 3V or 5V . | + | {{ : |
- | It has also LT6994 robust built in delay block timer chip that generateS the Geiger clicking sound to a regular buzzer. The LT6994 is a programmable delay block timer with a range of 1µs to 33.6 seconds. The LT6994 | + | [[ADI> |
- | the TimerBlox® family of versatile silicon timing devices. | + | |
- | A single resistor, RSET, programs an internal master | + | |
- | input-to-output | + | |
- | The circuit also has LEDs indicating radiation levels , reports counts per minute , | + | ==== Simplified Block Diagram ==== |
+ | {{ : | ||
+ | ==== Board Pinout ==== | ||
+ | The figure below shows the pins used as well as their corresponding functions. It can be seen that the output pin for the Geiger pulse can be set in four different locations. This allows flexibility in case other shields are used together with the CN0536. By default, JP1 is shorted and the Geiger pulse is read from GPIO33. Noting that some pins have specific alternate functions, all other unlabeled pins are free to be used. | ||
+ | {{ : | ||
- | |||
- | This user guide will discuss how to use the [[adi> | ||
- | |||
- | |||
- | |||
- | |||
- | |||
- | ======EVAL-CN0536-ARDZ attached to EVAL-ADICUP3029====== | ||
- | |||
- | |||
- | {{ : | ||
- | |||
- | |||
- | |||
- | |||
- | |||
- | |||
- | ====== Simplified functional block diagram ====== | ||
- | |||
- | |||
- | {{ : | ||
\\ | \\ | ||
+ | ====Video Guide==== | ||
+ | ===Unboxing and Theory of Operation=== | ||
+ | {{youtube> | ||
- | ===== General Setup ===== | + | ===== Device Driver Support and Software Demo ===== |
- | ==== Equipment | + | |
- | * [[adi>EVAL-CN0536-ARDZ|EVAL-CN0536-ARDZ | + | This [[resources: |
- | * [[adi> | + | |
- | * PC with a USB port and Windows 10 (32-bit) or higher | + | |
- | * +6V DC Power Supply or equivalent bench supply | + | |
- | * USB type A to micro USB type A cable | + | |
- | * CN0536 Evaluation Software | + | |
- | * Small Philips screwdriver | + | |
- | {{ : | ||
+ | {{ : | ||
+ | ===== Schematic, Layout, Bill of Materials ===== | ||
+ | <WRAP round 80% download> | ||
+ | [[https:// | ||
+ | * Schematic | ||
+ | * PCB Layout | ||
+ | * Allegro Project | ||
+ | * Bill of Materials | ||
+ | </ | ||
- | ====Peripheral Connectors ==== | + | ===== More Information and Useful Links ===== |
- | + | ||
- | All connector pinouts for the EVAL-CN0536-ARDZ are described in the table below. | + | |
- | + | ||
- | ^ Connector | + | |
- | ^ Arduino DIO High | 1 | SCL | I2C0_SCL/ | + | |
- | | ::: | 2 | SDA | I2C0_SDA/ | + | |
- | | ::: | 3 | AREF | VREF+ | NC | | + | |
- | | ::: | 4 | AGND | AGND (Analog ground) | + | |
- | | ::: | 5 | SCLK | SPI0_CLK/ | + | |
- | | ::: | 6 | MISO | SPI0_MISO/ | + | |
- | | ::: | 7 | MOSI | SPI0_MOSI/ | + | |
- | | ::: | 8 | CS | SPI0_CS1/ | + | |
- | | ::: | 9 | RDY | SPI0_RDY/ | + | |
- | | ::: | + | |
- | ^ Arduino DIO Low | 1 | IO08 | BPR0_TONE_N/ | + | |
- | | ::: | 2 | IO27 | TMR1_OUT/ | + | |
- | | ::: | 3 | IO33 | XINT0_WAKE3/ | + | |
- | | ::: | 4 | IO09 | BPR0_TONE_P/ | + | |
- | | ::: | 5 | IO13 | XINT0_WAKE2/ | + | |
- | | ::: | 6 | IO15 | XINT0_WAKE0/ | + | |
- | | ::: | 7 | TX | UART0_TX/ | + | |
- | | ::: | 8 | RX | UART0_RX/ | + | |
- | ^ Arduino Analog | + | |
- | | ::: | 2 | AIN1 | ADC0_VIN1/ | + | |
- | | ::: | 3 | AIN2 | ADC0_VIN2/ | + | |
- | | ::: | 4 | AIN3 | ADC0_VIN3/ | + | |
- | | ::: | 5 | AIN4 | ADC0_VIN4/ | + | |
- | | ::: | 6 | AIN5 | ADC0_VIN5/ | + | |
- | ^ Arduino Power | 1 | NC | - not connected - | NC | | + | |
- | | ::: | 2 | IOREF | +3.3V | IO_VREF (+3V3) | + | |
- | | ::: | 3 | RESET | SYS_HWRST_N | + | |
- | | ::: | 4 | 3.3V | +3.3V | NC | | + | |
- | | ::: | 5 | 5V | +5V | 5V | | + | |
- | | ::: | 6 | GND | DGND (Digital Ground) | + | |
- | | ::: | 7 | GND | DGND (Digital Ground) | + | |
- | | ::: | 8 | Vin | DC Barrel Jack Power +7V to +12V | +7.5V | | + | |
- | + | ||
- | + | ||
- | + | ||
- | === More Information and Useful Links ===== | + | |
- | * [[https:// | + | |
- | * [[ADI> | + | |
- | * [[ADI> | + | |
* [[ADI> | * [[ADI> | ||
- | * [[ADI> | + | * [[ADI> |
* [[ADI> | * [[ADI> | ||
- | * [[ADI> | + | * [[ADI> |
- | | + | |
- | + | ===== Registration | |
- | + | <WRAP round tip 80% > | |
- | + | Receive software update notifications, | |
- | + | ||
- | ====== Schematic, PCB Layout, Bill of Materials ====== | + | |
- | <WRAP round 80% download> | + | |
- | + | ||
- | [[adi>cn0536-designsupport|EVAL-CN0536-ARDZ | + | |
- | * Schematics | + | |
- | * PCB Layout | + | |
- | * Bill of Materials | + | |
- | * Allegro Project | + | |
- | + | ||
- | </ | + | |
- | ====== Software ====== | + | |
- | * [[resources: | + | |
- | + | ||
// End of Document // | // End of Document // |