This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0535:sdp-k1 [16 Jul 2021 08:08] – [Command Summary] John Neeko Garlitos | resources:eval:user-guides:circuits-from-the-lab:cn0535:sdp-k1 [27 Oct 2021 08:53] (current) – [SDP-K1] John Neeko Garlitos | ||
---|---|---|---|
Line 34: | Line 34: | ||
==== SDP-K1 ==== | ==== SDP-K1 ==== | ||
- | + | >>Shown below is the **CN0535 board** mounted on the **SDP-K1 board** via the Arduino headers. The SDP-K1 only requires a single Standard-A to type-C USB cable to connect to the PC. Both the orange Connected LED and green SYS PWR should light on the SDP-K1 if connected correctly. | |
- | Shown below is the **CN0535 board** mounted on the **SDP-K1 board** via the Arduino headers. The SDP-K1 only requires a single Standard-A to Mini-B USB cable to connect to the PC. Both the orange Connected LED and green SYS PWR should light on the SDP-K1 if connected correctly. | + | {{ : |
- | + | Note: For SDP-K1 Rev E and Below, a 6V wall-wart power is needed on P15. | |
- | {{ : | + | |
===== Software Setup ===== | ===== Software Setup ===== | ||
- | ==== Programming the SDP-K1 ==== | ||
- | Following are the steps then required to be completed to set up the [[adi> | ||
- | |||
- | - Download the [[adi> | ||
- | - Plug the USB cables from the PC into the **SDP-K1**. If installation was successful a new device named SDP-K1 should appear under 'This PC' in Windows File Explorer. {{ : | ||
- | - Download the AD7768_mbedos.SDP_K1.bin firmware. | ||
- | - Copy and paste or drag and drop the AD7768_mbedos.SDP_K1.bin file into the SDP-K1 device/ | ||
- | - If the download fails, a FAIL.TXT file will appear on the SDP-K1 device. | ||
- | - If the download is successful the .bin file will disappear from the SDP-K1 device and there will be no FAIL.TXT file. | ||
- | - Unplug the **SDP-K1 board** from the PC and plug it back in to hard reset the board and finalize installation. | ||
==== Importing the EVAL-CN0535-FMCZ MBED Example program ==== | ==== Importing the EVAL-CN0535-FMCZ MBED Example program ==== | ||
Line 55: | Line 44: | ||
- After having a acount, open the Example program for EVAL-CN0535-FMCZ https:// | - After having a acount, open the Example program for EVAL-CN0535-FMCZ https:// | ||
{{ : | {{ : | ||
+ | - | ||
+ | |||
+ | |||
+ | |||
==== Connecting to a serial terminal application ==== | ==== Connecting to a serial terminal application ==== | ||