Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:circuits-from-the-lab:cn0535:sdp-k1 [26 Oct 2021 15:06] – [Importing the EVAL-CN0535-FMCZ MBED Example program] John Neeko Garlitosresources:eval:user-guides:circuits-from-the-lab:cn0535:sdp-k1 [27 Oct 2021 08:53] (current) – [SDP-K1] John Neeko Garlitos
Line 34: Line 34:
  
 ==== SDP-K1 ==== ==== SDP-K1 ====
->For SDP-K1 Rev E and Below: 
->>Shown below is the **CN0535 board** mounted on the **SDP-K1 board** via the Arduino headers. The SDP-K1 only requires a single Standard-A to Mini-B USB cable to connect to the PC. Both the orange Connected LED and green SYS PWR should light on the SDP-K1 if connected correctly. 
-{{ :resources:eval:user-guides:circuits-from-the-lab:cn0535:setup_block_diagram.png |}} 
->For SDP-K1 Rev E and Up: 
 >>Shown below is the **CN0535 board** mounted on the **SDP-K1 board** via the Arduino headers. The SDP-K1 only requires a single Standard-A to type-C USB cable to connect to the PC. Both the orange Connected LED and green SYS PWR should light on the SDP-K1 if connected correctly. >>Shown below is the **CN0535 board** mounted on the **SDP-K1 board** via the Arduino headers. The SDP-K1 only requires a single Standard-A to type-C USB cable to connect to the PC. Both the orange Connected LED and green SYS PWR should light on the SDP-K1 if connected correctly.
 {{ :resources:eval:user-guides:circuits-from-the-lab:cn0535:setup_block_diagram2.png |}} {{ :resources:eval:user-guides:circuits-from-the-lab:cn0535:setup_block_diagram2.png |}}
 +Note: For SDP-K1 Rev E and Below, a 6V wall-wart power is needed on P15. 
 ===== Software Setup ===== ===== Software Setup =====
  
resources/eval/user-guides/circuits-from-the-lab/cn0535/sdp-k1.txt · Last modified: 27 Oct 2021 08:53 by John Neeko Garlitos