Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |
resources:eval:user-guides:circuits-from-the-lab:cn0535:sdp-k1 [26 Oct 2021 15:06] – [Importing the EVAL-CN0535-FMCZ MBED Example program] John Neeko Garlitos | resources:eval:user-guides:circuits-from-the-lab:cn0535:sdp-k1 [27 Oct 2021 08:53] (current) – [SDP-K1] John Neeko Garlitos |
---|
| |
==== SDP-K1 ==== | ==== SDP-K1 ==== |
>For SDP-K1 Rev E and Below: | |
>>Shown below is the **CN0535 board** mounted on the **SDP-K1 board** via the Arduino headers. The SDP-K1 only requires a single Standard-A to Mini-B USB cable to connect to the PC. Both the orange Connected LED and green SYS PWR should light on the SDP-K1 if connected correctly. | |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0535:setup_block_diagram.png |}} | |
>For SDP-K1 Rev E and Up: | |
>>Shown below is the **CN0535 board** mounted on the **SDP-K1 board** via the Arduino headers. The SDP-K1 only requires a single Standard-A to type-C USB cable to connect to the PC. Both the orange Connected LED and green SYS PWR should light on the SDP-K1 if connected correctly. | >>Shown below is the **CN0535 board** mounted on the **SDP-K1 board** via the Arduino headers. The SDP-K1 only requires a single Standard-A to type-C USB cable to connect to the PC. Both the orange Connected LED and green SYS PWR should light on the SDP-K1 if connected correctly. |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0535:setup_block_diagram2.png |}} | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0535:setup_block_diagram2.png |}} |
| Note: For SDP-K1 Rev E and Below, a 6V wall-wart power is needed on P15. |
===== Software Setup ===== | ===== Software Setup ===== |
| |