EVAL-CN0533-EBZ is a MEMS accelerometer (ADXL1002) vibration sensing solution with included analog 4-20 mA current loop interface circuitry, suitable for Condition-based Monitoring (CbM) applications. 4-20 mA current loop has been an industry analog signaling standard since 1950s. The main advantage of this signal standard is that there exists virtually no attenuation over long cables, therefore more robustness in EMI prone environments, such as industrial and factory settings. This reference design enables utilization of high bandwidth, ultralow noise MEMS accelerometers on a legacy 4-20 mA data acquisition (DAQ) systems for CbM applications.
The EVAL-CN0533-EBZ is very straightforward to setup. A cable, power supply (12-24 V), and a 4-20mA receiver are needed. For electrical setup:
The accelerometer used in this reference design, ADXL1002, is an ultra-low noise and high bandwidth sensor. To achieve the best performance, a proper mechanical design is required to deliver vibration signal from the measurement point to the sensor. Careful considerations in design of EVAL-CN0533-EBZ PCB has been taken to avoid vibration signal distortion to the sensor due to mechanical resonance of the PCB structure. To best deliver the vibration signal from the measurement point to the PCB, we have designed EVAL-XLMOUNT1. This mechanical interface is optimized to have a 3dB flat mechanical response of up to 20 kHz. Therefore, by utilization of EVAL-XLMOUNT1, the vibration signal will be adequately coupled with the sensor. The following steps describe how to use EVAL-XLMOUNT1 with EVAL-CN0533-EBZ.
EVAL-CN0533-EBZ Design & Integration Files
Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware. Register to receive all these great benefits and more!
End of Document