Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0511 [27 Jan 2023 09:08]
Joyce Velasco Replaced the obsolete Kuiper Linux page link
resources:eval:user-guides:circuits-from-the-lab:cn0511 [30 Jan 2023 02:30]
Joyce Velasco
Line 133: Line 133:
 ==== Downloading and Flashing Kuiper Linux Image on SD Card ==== ==== Downloading and Flashing Kuiper Linux Image on SD Card ====
  
-In order to control the **EVAL-CN0511-RPIZ** from the Raspberry Pi, you will need to install ADI Kuiper Linux on an SD card. Complete instructions,​ including where to download the SD card image, how to write it to the SD card, and how to configure the system are provided at **[[:​resources:​tools-software/linux-software/kuiper-linux |Kuiper Images]]**. Write the image and follow the system configuration procedure.+In order to control the **EVAL-CN0511-RPIZ** from the Raspberry Pi, you will need to install ADI Kuiper Linux on an SD card. Complete instructions,​ including where to download the SD card image, how to write it to the SD card, and how to configure the system are provided at **[[:​resources:​tools-software:linux-software:kuiper-linux |Kuiper Images]]**. Write the image and follow the system configuration procedure.
    
 {{ :​university:​labs:​software:​iio_intro_toolbox:​command_prompt.png?​400 |}} {{ :​university:​labs:​software:​iio_intro_toolbox:​command_prompt.png?​400 |}}
Line 141: Line 141:
 For the Linux kernel to identify the device connected to the expansion header, update the device tree overlay. A **Device Tree Overlay** contains information about additional connected hardware, the EVAL-CN0511-RPIZ for this case. The overlay file is already included in the SD card and just needs to be matched to the EVAL-CN0511-RPIZ. For the Linux kernel to identify the device connected to the expansion header, update the device tree overlay. A **Device Tree Overlay** contains information about additional connected hardware, the EVAL-CN0511-RPIZ for this case. The overlay file is already included in the SD card and just needs to be matched to the EVAL-CN0511-RPIZ.
  
-Follow the Hardware Configuration procedure under **Preparing the Image: Raspberry Pi** in the [[:​resources:​tools-software/linux-software/kuiper-linux |Kuiper Images]] page, substituting the following lines in **config.txt**:​+Follow the Hardware Configuration procedure under **Preparing the Image: Raspberry Pi** in the [[:​resources:​tools-software:linux-software:kuiper-linux |Kuiper Images]] page, substituting the following lines in **config.txt**:​
  
 This brings up the file in the terminal. Scroll down until the line that begins with "​dtoverlay"​ is found; then, whatever it currently is, change it to: This brings up the file in the terminal. Scroll down until the line that begins with "​dtoverlay"​ is found; then, whatever it currently is, change it to:
Line 294: Line 294:
   * [[:​resources:​tools-software:​linux-software:​pyadi-iio|PyADI-IIO Installation Guide]]   * [[:​resources:​tools-software:​linux-software:​pyadi-iio|PyADI-IIO Installation Guide]]
   * [[:​resources:​tools-software:​linux-software:​iio_oscilloscope|IIO Oscilloscope Installation Guide]]   * [[:​resources:​tools-software:​linux-software:​iio_oscilloscope|IIO Oscilloscope Installation Guide]]
-  * [[:​resources:​tools-software/linux-software/kuiper-linux |Kuiper Images]]+  * [[:​resources:​tools-software:linux-software:kuiper-linux |Kuiper Images]]
  
 ===== More Information and Useful Links  ===== ===== More Information and Useful Links  =====
resources/eval/user-guides/circuits-from-the-lab/cn0511.txt · Last modified: 30 Jan 2023 02:30 by Joyce Velasco