This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0508 [09 Mar 2022 20:55] – fix link Robin Getz | resources:eval:user-guides:circuits-from-the-lab:cn0508 [27 Jan 2023 09:03] – Replaced the obsolete Kuiper Linux page link Joyce Velasco | ||
---|---|---|---|
Line 198: | Line 198: | ||
===== Software Setup ===== | ===== Software Setup ===== | ||
==== Loading CN0508 Image on SD Card ==== | ==== Loading CN0508 Image on SD Card ==== | ||
- | In order to control the CN0508 from the Raspberry Pi, you will need to install ADI Kuiper Linux on an SD card. Complete instructions, | + | In order to control the CN0508 from the Raspberry Pi, you will need to install ADI Kuiper Linux on an SD card. Complete instructions, |
\\ | \\ | ||
Write the image and follow the system configuration procedure. | Write the image and follow the system configuration procedure. | ||
==== Configuring the SD Card ==== | ==== Configuring the SD Card ==== | ||
- | Follow the Hardware Configuration procedure under **Preparing the Image: Raspberry Pi** in the [[: | + | Follow the Hardware Configuration procedure under **Preparing the Image: Raspberry Pi** in the [: |
< | < |