This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:circuits-from-the-lab:cn0508 [27 Jan 2023 09:03] Joyce Velasco Replaced the obsolete Kuiper Linux page link |
resources:eval:user-guides:circuits-from-the-lab:cn0508 [30 Jan 2023 02:14] Joyce Velasco |
||
---|---|---|---|
Line 198: | Line 198: | ||
===== Software Setup ===== | ===== Software Setup ===== | ||
==== Loading CN0508 Image on SD Card ==== | ==== Loading CN0508 Image on SD Card ==== | ||
- | In order to control the CN0508 from the Raspberry Pi, you will need to install ADI Kuiper Linux on an SD card. Complete instructions, including where to download the SD card image, how to write it to the SD card, and how to configure the system are provided at **[[:resources:tools-software/linux-software/kuiper-linux |Kuiper Images]]**. | + | In order to control the CN0508 from the Raspberry Pi, you will need to install ADI Kuiper Linux on an SD card. Complete instructions, including where to download the SD card image, how to write it to the SD card, and how to configure the system are provided at **[[:resources:tools-software:linux-software:kuiper-linux |Kuiper Images]]**. |
\\ | \\ | ||
Write the image and follow the system configuration procedure. | Write the image and follow the system configuration procedure. | ||
==== Configuring the SD Card ==== | ==== Configuring the SD Card ==== | ||
- | Follow the Hardware Configuration procedure under **Preparing the Image: Raspberry Pi** in the [:resources:tools-software/linux-software/kuiper-linux |Kuiper Images]] page, substituting the following lines in **config.txt**: | + | Follow the Hardware Configuration procedure under **Preparing the Image: Raspberry Pi** in the [:resources:tools-software:linux-software:kuiper-linux |Kuiper Images]] page, substituting the following lines in **config.txt**: |
<code> | <code> |