Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0503 [17 Nov 2021 01:08] – [Optical Path 3] Brandon Busheyresources:eval:user-guides:circuits-from-the-lab:cn0503 [20 Sep 2022 15:24] (current) – adding nitrate demo link Brandon Bushey
Line 246: Line 246:
 ==== Optical Path 3 ==== ==== Optical Path 3 ====
 In optical path 3, the experiment shows nitrate detection using colorimetry. Using the API reagent found in nitrate test kits, a solution with a higher concentration of nitrate turns into a darker shade of red. As a result, the degree of absorbance of 615nm light decreases with the increasing nitrate concentration. In optical path 3, the experiment shows nitrate detection using colorimetry. Using the API reagent found in nitrate test kits, a solution with a higher concentration of nitrate turns into a darker shade of red. As a result, the degree of absorbance of 615nm light decreases with the increasing nitrate concentration.
-  * [[resources:eval:user-guides:circuits-from-the-lab:cn0503:nitrate|Optical Platform: Nitrate Measurement Demo (ADICUP3029 + EVAL-CN0503-ADRZ)]] //Coming Soon//\\ \\  +  * [[:resources:eval:user-guides:circuits-from-the-lab:cn0503:nitrate-measurement|Optical Platform: Nitrate Measurement Demo (ADICUP3029 + EVAL-CN0503-ADRZ)]]\\ \\ 
 ==== Optical Path 4 ==== ==== Optical Path 4 ====
 In optical path 4, the experiment shows turbidity measurements of cloudy water made by adding a a drop of milk and de-ionized water using 530nm light. In optical path 4, the experiment shows turbidity measurements of cloudy water made by adding a a drop of milk and de-ionized water using 530nm light.
Line 258: Line 257:
   * [[resources:eval:user-guides:circuits-from-the-lab:cn0503:colorimetry|Optical Platform: pH Measurement Demo (ADICUP3029 + EVAL-CN0503-ADRZ)]]   * [[resources:eval:user-guides:circuits-from-the-lab:cn0503:colorimetry|Optical Platform: pH Measurement Demo (ADICUP3029 + EVAL-CN0503-ADRZ)]]
   * [[resources:eval:user-guides:circuits-from-the-lab:cn0503:turbidity|Optical Platform: Turbidity Measurement Demo (ADICUP3029 + EVAL-CN0503-ADRZ)]]   * [[resources:eval:user-guides:circuits-from-the-lab:cn0503:turbidity|Optical Platform: Turbidity Measurement Demo (ADICUP3029 + EVAL-CN0503-ADRZ)]]
 +  * [[:resources:eval:user-guides:circuits-from-the-lab:cn0503:nitrate-measurement|Optical Platform: Nitrate Measurement Demo (ADICUP3029 + EVAL-CN0503-ADRZ)]]
  
 ===== Schematic, PCB Layout, Bill of Materials ===== ===== Schematic, PCB Layout, Bill of Materials =====
resources/eval/user-guides/circuits-from-the-lab/cn0503.txt · Last modified: 20 Sep 2022 15:24 by Brandon Bushey