Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0503:fluorescence [14 Jul 2021 16:40]
Brandon Bushey updated title
resources:eval:user-guides:circuits-from-the-lab:cn0503:fluorescence [02 Aug 2021 19:45] (current)
Angelo Nikko Catapang
Line 30: Line 30:
 <note important>​You can use either path 1 or 4 for fluorescence measurements. The steps outlined here will use path 1, and setting LED1, P1ASEL, and P1BSEL.</​note>​ <note important>​You can use either path 1 or 4 for fluorescence measurements. The steps outlined here will use path 1, and setting LED1, P1ASEL, and P1BSEL.</​note>​
   - Connect the 365nm LED Board and the 615nm LED Board to LED1.\\ {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0503:​fl_ledplacement.jpg?​nolink&​600 |}}   - Connect the 365nm LED Board and the 615nm LED Board to LED1.\\ {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0503:​fl_ledplacement.jpg?​nolink&​600 |}}
-  - Place the fluorescent filter into the slot in front of PD1B. and set the jumper connection as below:​\\ ​+  - Place the fluorescent filter into the slot in front of PD1B. and set the jumper connection as below:​\\ ​{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0503:​fl_fluorescentfilter.png?​400 |}}
  
 ^ Jumper Header ​           ^ Setting ​     ^ Image ^ ^ Jumper Header ​           ^ Setting ​     ^ Image ^
resources/eval/user-guides/circuits-from-the-lab/cn0503/fluorescence.txt · Last modified: 02 Aug 2021 19:45 by Angelo Nikko Catapang