resources:eval:user-guides:circuits-from-the-lab:cn0503:colorimetry [20 May 2021 15:18]
Angelo Nikko Catapang
resources:eval:user-guides:circuits-from-the-lab:cn0503:colorimetry [21 Jul 2021 08:48] (current)
Angelo Nikko Catapang
Line 1: Line 1:
-====== Optical Platform ​Colorimetry (EVAL-CN0503-ARDZ) ​======+====== Optical Platform: pH Measurement Demo ======
  
 Colorimetry can be used to determine the concentration of materials in a solution based on its absorbance. One application of colorimetry is pH measurement with the aid of a coloring reagent. This document details the steps in setting up the EVAL-CN0503-ARDZ for pH measurement. Colorimetry can be used to determine the concentration of materials in a solution based on its absorbance. One application of colorimetry is pH measurement with the aid of a coloring reagent. This document details the steps in setting up the EVAL-CN0503-ARDZ for pH measurement.
Line 28: Line 28:
  
 ^ Jumper Header ​           ^ Setting ​    ^ Image ^ ^ Jumper Header ​           ^ Setting ​    ^ Image ^
-| //LD2SEL and LD3SEL// ​   | Set to VARD | {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0503:​ld2sel_-_ard.png?​nolink&​400 ​|}} +| //LD2SEL and LD3SEL// ​   | Set to VARD | {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0503:​ld2sel_-_ard.png?​100 |}} {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0503:​ld3sel_-_ard.png?​100 |                              }}                                               | 
-| //​IOSEL// ​               | Set to ARD  | {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0503:​iosel_-_ard.png?​nolink&​400 |}} +| //​IOSEL// ​               | Set to ARD  | {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0503:​iosel_-_ard.png?​nolink&​100 |}}                          | 
-| //​P1.8V// ​               | Shorted ​    | {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0503:​p1.8v_-_ard.png?​nolink&​400 |}}+| //​P1.8V// ​               | Shorted ​    | {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0503:​p1.8v_-_ard.png?​nolink&​100 |}}                          |
  
 ==== Initial Connection and Setup ==== ==== Initial Connection and Setup ====
resources/eval/user-guides/circuits-from-the-lab/cn0503/colorimetry.1621516681.txt.gz · Last modified: 20 May 2021 15:18 by Angelo Nikko Catapang