This shows you the differences between two versions of the page.
Next revisionBoth sides next revision | |||
resources:eval:user-guides:circuits-from-the-lab:cn0503:colorimetry [26 Mar 2021 03:39] – created Angelo Nikko Catapang | resources:eval:user-guides:circuits-from-the-lab:cn0503:colorimetry [05 Apr 2021 10:58] – Angelo Nikko Catapang | ||
---|---|---|---|
Line 24: | Line 24: | ||
Before starting with these steps, please check the Hardware User Guide for the steps to assembling the EVAL-CN0503-ARDZ. Additionally, | Before starting with these steps, please check the Hardware User Guide for the steps to assembling the EVAL-CN0503-ARDZ. Additionally, | ||
- | * Configure the onboard jumper shunt connection as below: | + | |
+ | Configure the onboard jumper shunt connection as below: | ||
^ Jumper Header | ^ Jumper Header | ||
Line 47: | Line 48: | ||
- Place a prepared cuvette with the test sample to either path 2 and path 3. Check the Preparing Test Sample section on how to prepare a cuvette with the test sample and indicator. | - Place a prepared cuvette with the test sample to either path 2 and path 3. Check the Preparing Test Sample section on how to prepare a cuvette with the test sample and indicator. | ||
- Select either path 2 or path 3, set display mode to INS1, and press Start Measurement. By default the system was configured to use the measurement curve shown below. Check the Setting Measurement Curve section on how to set your own using spreadsheets and the advanced settings | - Select either path 2 or path 3, set display mode to INS1, and press Start Measurement. By default the system was configured to use the measurement curve shown below. Check the Setting Measurement Curve section on how to set your own using spreadsheets and the advanced settings | ||
+ | |||
+ | ===== Preparing Test Samples ===== | ||
+ | |||
+ | ===== Generating a Measurement Curve ===== |