This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0503:colorimetry [20 May 2021 15:18] – Angelo Nikko Catapang | resources:eval:user-guides:circuits-from-the-lab:cn0503:colorimetry [21 Jul 2021 08:48] (current) – Angelo Nikko Catapang | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Optical Platform | + | ====== Optical Platform: pH Measurement Demo ====== |
Colorimetry can be used to determine the concentration of materials in a solution based on its absorbance. One application of colorimetry is pH measurement with the aid of a coloring reagent. This document details the steps in setting up the EVAL-CN0503-ARDZ for pH measurement. | Colorimetry can be used to determine the concentration of materials in a solution based on its absorbance. One application of colorimetry is pH measurement with the aid of a coloring reagent. This document details the steps in setting up the EVAL-CN0503-ARDZ for pH measurement. | ||
Line 28: | Line 28: | ||
^ Jumper Header | ^ Jumper Header | ||
- | | //LD2SEL and LD3SEL// | + | | //LD2SEL and LD3SEL// |
- | | // | + | | // |
- | | // | + | | // |
==== Initial Connection and Setup ==== | ==== Initial Connection and Setup ==== |