Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:eval:user-guides:circuits-from-the-lab:cn0428 [08 Mar 2019 20:14] – Changed link to ADuCM355 code Scott Hunt | resources:eval:user-guides:circuits-from-the-lab:cn0428 [10 Jul 2019 17:40] – [(Optional) Programming the CN0428 with Custom Firmware] Scott Hunt |
---|
===== (Optional) Programming the CN0428 with Custom Firmware ===== | ===== (Optional) Programming the CN0428 with Custom Firmware ===== |
| |
The [[https://analog.com/cn0428|EVAL-CN0428-EBZ]] board ships pre-programmed with the default CN0428 firmware. However if the user wishes to modify the firmware for custom measurements, they need to download and install IAR ARM 8.30.2 (or above) workbench. Along with this the user also needs to download the ADuCM355 support package from the Source Code link in the [[cn0428#software|Software]] section. | The [[https://analog.com/cn0428|EVAL-CN0428-EBZ]] board ships pre-programmed with the default CN0428 firmware. However if the user wishes to modify the firmware for custom measurements, they need to download and install IAR Embedded Workbench for ARM 8.32 or higher. Along with this the user also needs to download the ADuCM355 support package from the Source Code link in the [[cn0428#software|Software]] section. |
| |
After installing the software package, there are two options how to program the [[https://analog.com/cn0428|EVAL-CN0428-EBZ]]:\\ | After installing the software package, there are two options how to program the [[https://analog.com/cn0428|EVAL-CN0428-EBZ]]:\\ |