This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0419 [13 Dec 2018 02:28] – req Trisha Cabildo | resources:eval:user-guides:circuits-from-the-lab:cn0419 [29 Jul 2021 05:37] (current) – [Registration] Zuedmar Arceo | ||
---|---|---|---|
Line 10: | Line 10: | ||
The EVAL-CN0419-EBZ board connects through a USB Type A Plug and is powered by the bus voltage from the USB port. | The EVAL-CN0419-EBZ board connects through a USB Type A Plug and is powered by the bus voltage from the USB port. | ||
- | {{ : | + | {{ : |
\\ | \\ | ||
---- | ---- | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
- | * [[adi>EVAL-CN0419-EBZ|EVAL-CN0419-EBZ Evaluation Board]] | + | * [[adi> |
* PC with the following //Minimum Requirements// | * PC with the following //Minimum Requirements// | ||
* PC, Mac, Linux computer, or other host that supports USB | * PC, Mac, Linux computer, or other host that supports USB | ||
Line 26: | Line 26: | ||
==== Block assignments ==== | ==== Block assignments ==== | ||
- | {{ : | + | {{ : |
- | * Terminal block **J1** is the USB Male plug to be inserted to USB port | + | * Terminal block **P1** is the USB Male plug to be inserted to USB port |
- | * Terminal block **J2** is the USB Female receptacle for the peripheral | + | * Terminal block **P2** is the USB Female receptacle for the peripheral |
* Terminal block **S1** is the switch for selection of speed operation (Full speed or Low speed) | * Terminal block **S1** is the switch for selection of speed operation (Full speed or Low speed) | ||
\\ | \\ | ||
+ | ==== Speed selection ==== | ||
+ | |||
+ | Peripheral devices run at one of three speeds, low (1.5 Mbps), full (12 Mbps), and high (480 Mbps). The [[adi> | ||
+ | - Low speed devices | ||
+ | * Examples: | ||
+ | * Bus rate: 1.5 Mb/s | ||
+ | - Full speed devices | ||
+ | * Examples: | ||
+ | * Bus rate: 12 Mb/s | ||
+ | |||
+ | The isolator is hardwired for the desired speed setting, either full speed or low speed. A switch at the upstream side allows the user to select between these speeds. To switch between the two modes, flip the actuator of S1 switch to FS mode as indicated in silkscreen for full speed operation and LS mode otherwise. | ||
+ | {{ : | ||
+ | Low speed operation | ||
+ | \\ | ||
+ | \\ | ||
+ | {{ : | ||
+ | Full speed operation | ||
+ | \\ | ||
+ | |||
==== Test setup ==== | ==== Test setup ==== | ||
{{ : | {{ : | ||
- Set the switch S1 to full speed or low speed operation depending on the peripheral specifications. | - Set the switch S1 to full speed or low speed operation depending on the peripheral specifications. | ||
- | - Connect the peripheral to J2 of the [[adi>EVAL-CN0419-EBZ|EVAL-CN0419-EBZ]] | + | - Connect the peripheral to P2 of the [[adi> |
- | - Plug J1 of the [[adi>EVAL-CN0419-EBZ|EVAL-CN0419-EBZ]] into the USB port of the PC | + | - Plug P1 of the [[adi> |
\\ | \\ | ||
==== Running the System ==== | ==== Running the System ==== | ||
- | + | - Make sure the setting for S1 is correct based on the peripheral device. | |
- | -After plugging | + | -Plug P1 of the board into the PC/host, the [[adi> |
- | -For devices like low speed mouse, keyboard and the like, low speed operation must be set | + | -The PC/host must recognize the peripheral connected to make sure the setup is working. |
- | -For devices such as USB flash drive, full speed operation must be set | + | |
- | -The PC must recognize the peripheral connected to make sure the setup is working | + | |
-Upon successful connection, you can now provide your peripheral the isolated power! | -Upon successful connection, you can now provide your peripheral the isolated power! | ||
Line 54: | Line 71: | ||
* [[ADI> | * [[ADI> | ||
- | * [[http:// | + | * [[adi>media/ |
* [[ADI> | * [[ADI> | ||
* [[ADI> | * [[ADI> | ||
Line 61: | Line 78: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[http:// | + | [[adi>media/ |
* Schematics | * Schematics | ||
* PCB Layout | * PCB Layout | ||
Line 67: | Line 84: | ||
* Allegro project | * Allegro project | ||
</ | </ | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ | ||
+ | |||
//End of Document// | //End of Document// | ||