resources:eval:user-guides:circuits-from-the-lab:cn0417 [21 Jan 2019 14:02]
Robin Getz add more info
resources:eval:user-guides:circuits-from-the-lab:cn0417 [30 Jul 2021 06:57] (current)
Zuedmar Arceo [Registration]
Line 13: Line 13:
  
 ===== Required Equipment ===== ===== Required Equipment =====
-  * [[adi>EVAL-CN0417-EBZ|EVAL-CN0417-EBZ ​Evaluation ​Board]]+  * [[adi>​CN0417|EVAL-CN0417-EBZ Board]]
   * RF Signal Source (like the [[adi>​PlutoSDR]])   * RF Signal Source (like the [[adi>​PlutoSDR]])
   * Micro-USB power adaptor or Micro-USB to USB cable   * Micro-USB power adaptor or Micro-USB to USB cable
Line 27: Line 27:
 ==== Test setup ==== ==== Test setup ====
 {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0417:​10-31-2018_10-51-55_am.png?​nolink&​600 |}}\\ {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0417:​10-31-2018_10-51-55_am.png?​nolink&​600 |}}\\
-  ​- Connect the RF output of the RF signal source to J1 of the [[adi>​EVAL-CN0417-EBZ|EVAL-CN0417-EBZ Evaluation Board]] +  - Plug in the micro-USB end of the micro-USB cable or power adapter to P1 of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] 
-  - Connect J2 of the [[adi>​EVAL-CN0417-EBZ|EVAL-CN0417-EBZ Evaluation Board]] to desired DUT or equipment needing the amplifier signal +  - Plug the other end of the cable to a power outlet or a PC USB port providing at least 500 mA.
-  ​- Plug in the micro-USB end of the micro-USB cable or power adapter to P1 of the [[adi>EVAL-CN0417-EBZ|EVAL-CN0417-EBZ ​Evaluation ​Board]] +
-  - Plug the other end of the cable to a power outlet or a PC USB port.+
   - An LED light will turn on indicating the board is on and is in operation.   - An LED light will turn on indicating the board is on and is in operation.
 +  - Connect the RF output of the RF signal source to J1 of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]]
 +  - Connect J2 of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] to desired DUT or equipment needing the amplifier signal
  
 ==== Running the System ==== ==== Running the System ====
-  -After completing the setup, the [[adi>EVAL-CN0417-EBZ|EVAL-CN0417-EBZ ​Evaluation ​Board]] will automatically turn on and output the amplified version of the input.+  -After completing the setup, the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] will automatically turn on and output the amplified version of the input.
  
 ==== Normal Operation ==== ==== Normal Operation ====
Line 40: Line 40:
 {{  :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0417.png?​300|}} {{  :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0417.png?​300|}}
 For normal operation, connect: For normal operation, connect:
-  ​- Connect the RF output of the Pluto SDR to J1 of the [[adi>​EVAL-CN0417-EBZ|EVAL-CN0417-EBZ Board]] +  - Connect P1 (micro USB) connector of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] into a PC USB port or 5V USB charger.
-  - Connect J2 of the [[adi>​EVAL-CN0417-EBZ|EVAL-CN0417-EBZ Board]] to an antenna (ensure the antenna can dissipate 1W) +
-  ​- Connect P1 (micro USB) connector of the [[adi>EVAL-CN0417-EBZ|EVAL-CN0417-EBZ Board]] into a PC USB port or 5V USB charger.+
   - An LED light will turn on indicating the board is on and is in operation.   - An LED light will turn on indicating the board is on and is in operation.
 +  - Connect the RF output of the Pluto SDR to J1 of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]]
 +  - Connect J2 of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] to an antenna (ensure the antenna can dissipate 1W)
  
 ------- -------
Line 49: Line 49:
 ===== WARNING ===== ===== WARNING =====
  
-<WRAP alert>​Connecting the  [[adi>EVAL-CN0417-EBZ|EVAL-CN0417-EBZ Board]] directly to the Pluto SDR input (Rx) may exceed the absolute maximum ratings for the RF Input (which is +2.5 dBm). Doing this may permanently damage the PlutoSDR input. Never do this for any reason.+<WRAP alert>​Connecting the  [[adi>​CN0417|EVAL-CN0417-EBZ Board]] directly to the Pluto SDR input (Rx) may exceed the absolute maximum ratings for the RF Input (which is +2.5 dBm). Doing this may permanently damage the PlutoSDR input. Never do this for any reason.
  
 {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0417:​pluto_setup_1.jpg?​nolink&​900|}} {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0417:​pluto_setup_1.jpg?​nolink&​900|}}
  
-We test the [[adi>EVAL-CN0417-EBZ|EVAL-CN0417-EBZ Board]] in this configuration,​ by ensuring the Tx attenuator is set to attenuation of 30dB or more. This ensures the gain of +20dB from the  [[adi>EVAL-CN0417-EBZ|EVAL-CN0417-EBZ Board]] will not exceed the maximum ratings for the RF Input.+We test the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] in this configuration,​ by ensuring the Tx attenuator is set to attenuation of 30dB or more. This ensures the gain of +20dB from the  [[adi>​CN0417|EVAL-CN0417-EBZ Board]] will not exceed the maximum ratings for the RF Input.
  
 Never do this in normal operation. Never do this in normal operation.
Line 62: Line 62:
 <WRAP download>​ <WRAP download>​
   * [[ADI>​CN0417|CN0417 Circuit Note Page]]   * [[ADI>​CN0417|CN0417 Circuit Note Page]]
-  * [[http://​www.analog.com/​media/​en/​reference-design-documentation/​design-integration-files/​CN0417-DesignSupport.zip|CN0417 Design Support Package]]+  * [[adi>media/​en/​reference-design-documentation/​design-integration-files/​CN0417-DesignSupport.zip|CN0417 Design Support Package]] 
 +  * [[/​university/​tools/​pluto/​users/​amp|Test Results]]
   * [[ADI>​ADL5606|ADL5606 Product Page]]   * [[ADI>​ADL5606|ADL5606 Product Page]]
   * [[ADI>​LTM8045|LTM8045 Product Page]]   * [[ADI>​LTM8045|LTM8045 Product Page]]
Line 70: Line 71:
  
 <WRAP round 80% download>​ <WRAP round 80% download>​
-[[http://​www.analog.com/​media/​en/​reference-design-documentation/​design-integration-files/​CN0417-DesignSupport.zip|EVAL-CN0417-SDPZ Design & Integration Files]]+[[adi>media/​en/​reference-design-documentation/​design-integration-files/​CN0417-DesignSupport.zip|EVAL-CN0417-SDPZ Design & Integration Files]]
   * Schematics ​   * Schematics ​
   * PCB Layout ​   * PCB Layout ​
Line 77: Line 78:
 </​WRAP>​ </​WRAP>​
  
 +=====Registration===== ​
 +<WRAP round tip 80% >
 +Receive software update notifications,​ documentation updates, view the latest videos, and more when you register your hardware. ​ [[reg>​EVAL-CN0417-EBZ?&​v=RevC|Register]] to receive all these great benefits and more!
 +</​WRAP>​
 +
 +//End of Document//
resources/eval/user-guides/circuits-from-the-lab/cn0417.1548075779.txt.gz · Last modified: 21 Jan 2019 14:02 by Robin Getz