Last revision Both sides next revision
resources:eval:user-guides:circuits-from-the-lab:cn0417 [22 Jan 2019 07:35]
Robin Getz fix links
resources:eval:user-guides:circuits-from-the-lab:cn0417 [03 Jan 2021 21:56]
Robin Getz fix links
Line 27: Line 27:
 ==== Test setup ==== ==== Test setup ====
 {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0417:​10-31-2018_10-51-55_am.png?​nolink&​600 |}}\\ {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0417:​10-31-2018_10-51-55_am.png?​nolink&​600 |}}\\
-  - Connect the RF output of the RF signal source to J1 of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] 
-  - Connect J2 of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] to desired DUT or equipment needing the amplifier signal 
   - Plug in the micro-USB end of the micro-USB cable or power adapter to P1 of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]]   - Plug in the micro-USB end of the micro-USB cable or power adapter to P1 of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]]
-  - Plug the other end of the cable to a power outlet or a PC USB port.+  - Plug the other end of the cable to a power outlet or a PC USB port providing at least 500 mA.
   - An LED light will turn on indicating the board is on and is in operation.   - An LED light will turn on indicating the board is on and is in operation.
 +  - Connect the RF output of the RF signal source to J1 of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]]
 +  - Connect J2 of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] to desired DUT or equipment needing the amplifier signal
  
 ==== Running the System ==== ==== Running the System ====
Line 40: Line 40:
 {{  :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0417.png?​300|}} {{  :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0417.png?​300|}}
 For normal operation, connect: For normal operation, connect:
-  - Connect the RF output of the Pluto SDR to J1 of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] 
-  - Connect J2 of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] to an antenna (ensure the antenna can dissipate 1W) 
   - Connect P1 (micro USB) connector of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] into a PC USB port or 5V USB charger.   - Connect P1 (micro USB) connector of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] into a PC USB port or 5V USB charger.
   - An LED light will turn on indicating the board is on and is in operation.   - An LED light will turn on indicating the board is on and is in operation.
 +  - Connect the RF output of the Pluto SDR to J1 of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]]
 +  - Connect J2 of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] to an antenna (ensure the antenna can dissipate 1W)
  
 ------- -------
Line 62: Line 62:
 <WRAP download>​ <WRAP download>​
   * [[ADI>​CN0417|CN0417 Circuit Note Page]]   * [[ADI>​CN0417|CN0417 Circuit Note Page]]
-  * [[http://​www.analog.com/​media/​en/​reference-design-documentation/​design-integration-files/​CN0417-DesignSupport.zip|CN0417 Design Support Package]]+  * [[adi>media/​en/​reference-design-documentation/​design-integration-files/​CN0417-DesignSupport.zip|CN0417 Design Support Package]]
   * [[/​university/​tools/​pluto/​users/​amp|Test Results]]   * [[/​university/​tools/​pluto/​users/​amp|Test Results]]
   * [[ADI>​ADL5606|ADL5606 Product Page]]   * [[ADI>​ADL5606|ADL5606 Product Page]]
Line 71: Line 71:
  
 <WRAP round 80% download>​ <WRAP round 80% download>​
-[[http://​www.analog.com/​media/​en/​reference-design-documentation/​design-integration-files/​CN0417-DesignSupport.zip|EVAL-CN0417-SDPZ Design & Integration Files]]+[[adi>media/​en/​reference-design-documentation/​design-integration-files/​CN0417-DesignSupport.zip|EVAL-CN0417-SDPZ Design & Integration Files]]
   * Schematics ​   * Schematics ​
   * PCB Layout ​   * PCB Layout ​
resources/eval/user-guides/circuits-from-the-lab/cn0417.txt · Last modified: 30 Jul 2021 06:57 by Zuedmar Arceo