resources:eval:user-guides:circuits-from-the-lab:cn0417 [21 Jan 2019 11:56]
Robin Getz [Do not do this]
resources:eval:user-guides:circuits-from-the-lab:cn0417 [30 Jul 2021 06:57]
Zuedmar Arceo [Registration]
Line 1: Line 1:
 ====== CN0417 Evaluation Board Guide ====== ====== CN0417 Evaluation Board Guide ======
 +
 ===== Overview ===== ===== Overview =====
-[[ADI>​CN0417]] is a small USB powered RF power amplifier optimized for 2400 MHz operation. The amplifier typically provides 20 dB of gain through its RF band of operation, boosting signals for various ​ communication protocols such as ISM, MC-GSM, W-CDMA, TD-SCDMA and LTE. It requires 5V USB supply for normal operation. The input and output, both populated with edge mounted SMA connectors, are dc blocked and matched to 50 Ω for ease of use. + 
 +[[adi>​CN0417]] is a small USB powered RF power amplifier optimized for 2400 MHz operation. The amplifier typically provides 20 dB of gain through its RF band of operation, boosting signals for various ​ communication protocols such as ISM, MC-GSM, W-CDMA, TD-SCDMA and LTE. It requires 5V USB supply for normal operation. The input and output, both populated with edge mounted SMA connectors, are dc blocked and matched to 50 Ω for ease of use. More information on this board can be found at [[/​university/​tools/​pluto/​users/​amp|PlutoSDR Amplifier]].
  
 The [[ADI>​ADL5606]] is a broadband, two-stage, 1 W RF driver amplifier that operates over a frequency range of 1800 MHz to 2700 MHz. The device can be used in a wide variety of wired and wireless communication protocols, including ISM, MC-GSM, W-CDMA, TD-SCDMA, and LTE.  The [[ADI>​ADL5606]] is a broadband, two-stage, 1 W RF driver amplifier that operates over a frequency range of 1800 MHz to 2700 MHz. The device can be used in a wide variety of wired and wireless communication protocols, including ISM, MC-GSM, W-CDMA, TD-SCDMA, and LTE. 
Line 9: Line 11:
 The EVAL-CN0417-EBZ board connects through SMA and is powered by the bus voltage from the USB port.\\ The EVAL-CN0417-EBZ board connects through SMA and is powered by the bus voltage from the USB port.\\
 {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0417:​block_diagram3.png?​nolink&​900 |}} {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0417:​block_diagram3.png?​nolink&​900 |}}
-\\ +
-----+
 ===== Required Equipment ===== ===== Required Equipment =====
-  * [[adi>EVAL-CN0417-EBZ|EVAL-CN0417-EBZ ​Evaluation ​Board]] +  * [[adi>​CN0417|EVAL-CN0417-EBZ Board]] 
-  * RF Signal Source+  * RF Signal Source ​(like the [[adi>​PlutoSDR]])
   * Micro-USB power adaptor or Micro-USB to USB cable   * Micro-USB power adaptor or Micro-USB to USB cable
-  * SMA to SMA cable 
  
----- 
 ===== General Setup ===== ===== General Setup =====
 +
 ==== Block assignments ==== ==== Block assignments ====
 {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0417:​revb_blockd.jpg?​nolink&​700 |}}\\ {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0417:​revb_blockd.jpg?​nolink&​700 |}}\\
-  * Terminal block **J1** is the SMA connector for RF input +  * Terminal block **J1** is the SMA female ​connector for RF input, and would normally be connected to an SDR. 
-  * Terminal block **J2** is the SMA connector for RF output+  * Terminal block **J2** is the SMA male connector for RF output, and would normally be connected to an antenna
   * Terminal block **P1** is the micro USB port to provide power to the board   * Terminal block **P1** is the micro USB port to provide power to the board
  
-\\ 
 ==== Test setup ==== ==== Test setup ====
 {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0417:​10-31-2018_10-51-55_am.png?​nolink&​600 |}}\\ {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0417:​10-31-2018_10-51-55_am.png?​nolink&​600 |}}\\
-  ​- Connect the RF output of the RF signal source to J1 of the [[adi>​EVAL-CN0417-EBZ|EVAL-CN0417-EBZ Evaluation Board]] +  - Plug in the micro-USB end of the micro-USB cable or power adapter ​to P1 of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] 
-  - Connect J2 of the [[adi>​EVAL-CN0417-EBZ|EVAL-CN0417-EBZ Evaluation Board]] to desired DUT or equipment needing the amplifier signal +  - Plug the other end of the cable to a power outlet or a PC USB port providing at least 500 mA.
-  ​- Plug in the micro-USB end of the micro-USB cable or power adaptor ​to P1 of the [[adi>EVAL-CN0417-EBZ|EVAL-CN0417-EBZ ​Evaluation ​Board]] +
-  - Plug the other end of the cable to a power outlet or a PC USB port.+
   - An LED light will turn on indicating the board is on and is in operation.   - An LED light will turn on indicating the board is on and is in operation.
-\\+  - Connect the RF output of the RF signal source to J1 of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] 
 +  - Connect J2 of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] to desired DUT or equipment needing the amplifier signal
  
 ==== Running the System ==== ==== Running the System ====
-  -After completing the setup, the [[adi>EVAL-CN0417-EBZ|EVAL-CN0417-EBZ ​Evaluation ​Board]] will automatically turn on and output the amplified version of the input. +  -After completing the setup, the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] will automatically turn on and output the amplified version of the input. 
-\\ + 
-----+==== Normal Operation ==== 
 + 
 +{{  :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0417.png?​300|}} 
 +For normal operation, connect: 
 +  - Connect P1 (micro USB) connector of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] into a PC USB port or 5V USB charger. 
 +  - An LED light will turn on indicating the board is on and is in operation. 
 +  - Connect the RF output of the Pluto SDR to J1 of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] 
 +  - Connect J2 of the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] to an antenna (ensure the antenna can dissipate 1W) 
 + 
 +------- 
 ===== WARNING ===== ===== WARNING =====
  
-<WRAP alert>​Connecting the  [[adi>EVAL-CN0417-EBZ|EVAL-CN0417-EBZ Board]] directly to the Pluto SDR input (Rx) may exceed the absolute maximum ratings for the RF Input (which is +2.5 dBm). Doing this may permanently damage the PlutoSDR input.+<WRAP alert>​Connecting the  [[adi>​CN0417|EVAL-CN0417-EBZ Board]] directly to the Pluto SDR input (Rx) may exceed the absolute maximum ratings for the RF Input (which is +2.5 dBm). Doing this may permanently damage the PlutoSDR input. ​Never do this for any reason. 
 + 
 +{{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0417:​pluto_setup_1.jpg?​nolink&​900|}} 
 + 
 +We test the [[adi>​CN0417|EVAL-CN0417-EBZ Board]] in this configuration,​ by ensuring the Tx attenuator is set to attenuation of 30dB or more. This ensures the gain of +20dB from the  [[adi>​CN0417|EVAL-CN0417-EBZ Board]] will not exceed the maximum ratings for the RF Input. 
 + 
 +Never do this in normal operation. 
 +</​WRAP>​
  
-{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0417:​pluto_setup_1.jpg?​nolink&​900|}} 
- </​WRAP>​ 
 ===== More Information and Useful Links  ===== ===== More Information and Useful Links  =====
-  * [[ftp://​ftp.analog.com/​pub/​cftl/​CN0417/​|CN0417 Evaluation Software]]+ 
 +<WRAP download>​
   * [[ADI>​CN0417|CN0417 Circuit Note Page]]   * [[ADI>​CN0417|CN0417 Circuit Note Page]]
-  * [[http://​www.analog.com/​media/​en/​reference-design-documentation/​design-integration-files/​CN0417-DesignSupport.zip|CN0417 Design Support Package]]+  * [[adi>media/​en/​reference-design-documentation/​design-integration-files/​CN0417-DesignSupport.zip|CN0417 Design Support Package]] 
 +  * [[/​university/​tools/​pluto/​users/​amp|Test Results]]
   * [[ADI>​ADL5606|ADL5606 Product Page]]   * [[ADI>​ADL5606|ADL5606 Product Page]]
   * [[ADI>​LTM8045|LTM8045 Product Page]]   * [[ADI>​LTM8045|LTM8045 Product Page]]
 +</​WRAP>​
  
 ===== Schematic, PCB Layout, Bill of Materials ===== ===== Schematic, PCB Layout, Bill of Materials =====
  
 <WRAP round 80% download>​ <WRAP round 80% download>​
-[[http://​www.analog.com/​media/​en/​reference-design-documentation/​design-integration-files/​CN0417-DesignSupport.zip|EVAL-CN0417-SDPZ Design & Integration Files]]+[[adi>media/​en/​reference-design-documentation/​design-integration-files/​CN0417-DesignSupport.zip|EVAL-CN0417-SDPZ Design & Integration Files]]
   * Schematics ​   * Schematics ​
   * PCB Layout ​   * PCB Layout ​
Line 62: Line 78:
 </​WRAP>​ </​WRAP>​
  
-//End of Document//+=====Registration=====  
 +<WRAP round tip 80% > 
 +Receive software update notifications,​ documentation updates, view the latest videos, and more when you register your hardware. ​ [[reg>​EVAL-CN0417-EBZ?&​v=RevC|Register]] to receive all these great benefits and more! 
 +</WRAP>
  
 +//End of Document//
resources/eval/user-guides/circuits-from-the-lab/cn0417.txt · Last modified: 30 Jul 2021 06:57 by Zuedmar Arceo