Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision |
resources:eval:user-guides:circuits-from-the-lab:cn0417 [21 Jan 2019 11:41] – [Sample Setup] Robin Getz | resources:eval:user-guides:circuits-from-the-lab:cn0417 [30 Jul 2021 06:57] – [Registration] Zuedmar Arceo |
---|
====== CN0417 Evaluation Board Guide ====== | ====== CN0417 Evaluation Board Guide ====== |
| |
===== Overview ===== | ===== Overview ===== |
[[ADI>CN0417]] is a small USB powered RF power amplifier optimized for 2400 MHz operation. The amplifier typically provides 20 dB of gain through its RF band of operation, boosting signals for various communication protocols such as ISM, MC-GSM, W-CDMA, TD-SCDMA and LTE. It requires 5V USB supply for normal operation. The input and output, both populated with edge mounted SMA connectors, are dc blocked and matched to 50 Ω for ease of use. | |
| [[adi>CN0417]] is a small USB powered RF power amplifier optimized for 2400 MHz operation. The amplifier typically provides 20 dB of gain through its RF band of operation, boosting signals for various communication protocols such as ISM, MC-GSM, W-CDMA, TD-SCDMA and LTE. It requires 5V USB supply for normal operation. The input and output, both populated with edge mounted SMA connectors, are dc blocked and matched to 50 Ω for ease of use. More information on this board can be found at [[/university/tools/pluto/users/amp|PlutoSDR Amplifier]]. |
| |
The [[ADI>ADL5606]] is a broadband, two-stage, 1 W RF driver amplifier that operates over a frequency range of 1800 MHz to 2700 MHz. The device can be used in a wide variety of wired and wireless communication protocols, including ISM, MC-GSM, W-CDMA, TD-SCDMA, and LTE. | The [[ADI>ADL5606]] is a broadband, two-stage, 1 W RF driver amplifier that operates over a frequency range of 1800 MHz to 2700 MHz. The device can be used in a wide variety of wired and wireless communication protocols, including ISM, MC-GSM, W-CDMA, TD-SCDMA, and LTE. |
The EVAL-CN0417-EBZ board connects through SMA and is powered by the bus voltage from the USB port.\\ | The EVAL-CN0417-EBZ board connects through SMA and is powered by the bus voltage from the USB port.\\ |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0417:block_diagram3.png?nolink&900 |}} | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0417:block_diagram3.png?nolink&900 |}} |
\\ | |
---- | |
===== Required Equipment ===== | ===== Required Equipment ===== |
* [[adi>EVAL-CN0417-EBZ|EVAL-CN0417-EBZ Evaluation Board]] | * [[adi>CN0417|EVAL-CN0417-EBZ Board]] |
* RF Signal Source | * RF Signal Source (like the [[adi>PlutoSDR]]) |
* Micro-USB power adaptor or Micro-USB to USB cable | * Micro-USB power adaptor or Micro-USB to USB cable |
* SMA to SMA cable | |
| |
---- | |
===== General Setup ===== | ===== General Setup ===== |
| |
==== Block assignments ==== | ==== Block assignments ==== |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0417:revb_blockd.jpg?nolink&700 |}}\\ | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0417:revb_blockd.jpg?nolink&700 |}}\\ |
* Terminal block **J1** is the SMA connector for RF input | * Terminal block **J1** is the SMA female connector for RF input, and would normally be connected to an SDR. |
* Terminal block **J2** is the SMA connector for RF output | * Terminal block **J2** is the SMA male connector for RF output, and would normally be connected to an antenna |
* Terminal block **P1** is the micro USB port to provide power to the board | * Terminal block **P1** is the micro USB port to provide power to the board |
| |
\\ | |
==== Test setup ==== | ==== Test setup ==== |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0417:10-31-2018_10-51-55_am.png?nolink&600 |}}\\ | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0417:10-31-2018_10-51-55_am.png?nolink&600 |}}\\ |
- Connect the RF output of the RF signal source to J1 of the [[adi>EVAL-CN0417-EBZ|EVAL-CN0417-EBZ Evaluation Board]] | - Plug in the micro-USB end of the micro-USB cable or power adapter to P1 of the [[adi>CN0417|EVAL-CN0417-EBZ Board]] |
- Connect J2 of the [[adi>EVAL-CN0417-EBZ|EVAL-CN0417-EBZ Evaluation Board]] to desired DUT or equipment needing the amplifier signal | - Plug the other end of the cable to a power outlet or a PC USB port providing at least 500 mA. |
- Plug in the micro-USB end of the micro-USB cable or power adaptor to P1 of the [[adi>EVAL-CN0417-EBZ|EVAL-CN0417-EBZ Evaluation Board]] | |
- Plug the other end of the cable to a power outlet or a PC USB port. | |
- An LED light will turn on indicating the board is on and is in operation. | - An LED light will turn on indicating the board is on and is in operation. |
\\ | - Connect the RF output of the RF signal source to J1 of the [[adi>CN0417|EVAL-CN0417-EBZ Board]] |
| - Connect J2 of the [[adi>CN0417|EVAL-CN0417-EBZ Board]] to desired DUT or equipment needing the amplifier signal |
| |
==== Running the System ==== | ==== Running the System ==== |
-After completing the setup, the [[adi>EVAL-CN0417-EBZ|EVAL-CN0417-EBZ Evaluation Board]] will automatically turn on and output the amplified version of the input. | -After completing the setup, the [[adi>CN0417|EVAL-CN0417-EBZ Board]] will automatically turn on and output the amplified version of the input. |
\\ | |
---- | |
===== Do not do this ===== | |
| |
<WRAP important>connecting your Pluto like this will cause the Rx to blow up. Never do it. </WRAP> | ==== Normal Operation ==== |
| |
| {{ :resources:eval:user-guides:circuits-from-the-lab:cn0417.png?300|}} |
| For normal operation, connect: |
| - Connect P1 (micro USB) connector of the [[adi>CN0417|EVAL-CN0417-EBZ Board]] into a PC USB port or 5V USB charger. |
| - An LED light will turn on indicating the board is on and is in operation. |
| - Connect the RF output of the Pluto SDR to J1 of the [[adi>CN0417|EVAL-CN0417-EBZ Board]] |
| - Connect J2 of the [[adi>CN0417|EVAL-CN0417-EBZ Board]] to an antenna (ensure the antenna can dissipate 1W) |
| |
| ------- |
| |
| ===== WARNING ===== |
| |
| <WRAP alert>Connecting the [[adi>CN0417|EVAL-CN0417-EBZ Board]] directly to the Pluto SDR input (Rx) may exceed the absolute maximum ratings for the RF Input (which is +2.5 dBm). Doing this may permanently damage the PlutoSDR input. Never do this for any reason. |
| |
| {{:resources:eval:user-guides:circuits-from-the-lab:cn0417:pluto_setup_1.jpg?nolink&900|}} |
| |
| We test the [[adi>CN0417|EVAL-CN0417-EBZ Board]] in this configuration, by ensuring the Tx attenuator is set to attenuation of 30dB or more. This ensures the gain of +20dB from the [[adi>CN0417|EVAL-CN0417-EBZ Board]] will not exceed the maximum ratings for the RF Input. |
| |
| Never do this in normal operation. |
| </WRAP> |
| |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0417:pluto_setup_1.jpg?nolink&900 |}}\\ | |
You can use the [[adi>EVAL-CN0417-EBZ|EVAL-CN0417-EBZ Evaluation Board]] with [[adi>ADALM-PLUTO|ADALM-PLUTO]] to boost the transmitted signal. It has a typical gain of 20 at 2400 MHz. | |
---- | |
===== More Information and Useful Links ===== | ===== More Information and Useful Links ===== |
* [[ftp://ftp.analog.com/pub/cftl/CN0417/|CN0417 Evaluation Software]] | |
| <WRAP download> |
* [[ADI>CN0417|CN0417 Circuit Note Page]] | * [[ADI>CN0417|CN0417 Circuit Note Page]] |
* [[http://www.analog.com/media/en/reference-design-documentation/design-integration-files/CN0417-DesignSupport.zip|CN0417 Design Support Package]] | * [[adi>media/en/reference-design-documentation/design-integration-files/CN0417-DesignSupport.zip|CN0417 Design Support Package]] |
| * [[/university/tools/pluto/users/amp|Test Results]] |
* [[ADI>ADL5606|ADL5606 Product Page]] | * [[ADI>ADL5606|ADL5606 Product Page]] |
* [[ADI>LTM8045|LTM8045 Product Page]] | * [[ADI>LTM8045|LTM8045 Product Page]] |
| </WRAP> |
| |
===== Schematic, PCB Layout, Bill of Materials ===== | ===== Schematic, PCB Layout, Bill of Materials ===== |
| |
<WRAP round 80% download> | <WRAP round 80% download> |
[[http://www.analog.com/media/en/reference-design-documentation/design-integration-files/CN0417-DesignSupport.zip|EVAL-CN0417-SDPZ Design & Integration Files]] | [[adi>media/en/reference-design-documentation/design-integration-files/CN0417-DesignSupport.zip|EVAL-CN0417-SDPZ Design & Integration Files]] |
* Schematics | * Schematics |
* PCB Layout | * PCB Layout |
</WRAP> | </WRAP> |
| |
//End of Document// | =====Registration===== |
| <WRAP round tip 80% > |
| Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware. [[reg>EVAL-CN0417-EBZ?&v=RevC|Register]] to receive all these great benefits and more! |
| </WRAP> |
| |
| //End of Document// |