Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0372 [10 Jul 2018 20:32]
Motoko Hunt [More Information and Useful Links]
resources:eval:user-guides:circuits-from-the-lab:cn0372 [03 Jan 2021 22:03]
Robin Getz fix links
Line 7: Line 7:
 The [[ADI>​AD7091R-5]] accepts the analog signals, buffered or unbuffered, and performs data conversion. ​ The [[ADI>​ADA4805-1]] is an optional buffer which can be used for all input channels because of an access to the multiplexer output of the [[ADI>​AD7091R-5]]. The [[ADI>​ADP5090]] harvests charge from a photovoltaic cell to generate the system DC supply rails. Another option provided to power the board is with the [[ADI>​ADP1607]]. A CR2032 battery connector is available to provide either the input to the [[ADI>​ADP1607]] or accelerate the cold start of the [[ADI>​ADP5090]]. The [[ADI>​AD7091R-5]] accepts the analog signals, buffered or unbuffered, and performs data conversion. ​ The [[ADI>​ADA4805-1]] is an optional buffer which can be used for all input channels because of an access to the multiplexer output of the [[ADI>​AD7091R-5]]. The [[ADI>​ADP5090]] harvests charge from a photovoltaic cell to generate the system DC supply rails. Another option provided to power the board is with the [[ADI>​ADP1607]]. A CR2032 battery connector is available to provide either the input to the [[ADI>​ADP1607]] or accelerate the cold start of the [[ADI>​ADP5090]].
  
-This user guide will discuss how to operate the [[http://​www.analog.com/​en/​design-center/​evaluation-hardware-and-software/​evaluation-boards-kits/​EVAL_SDP-PMOD.html#​eb-overview| SDP-PMD-IB1Z]],​ [[http://​www.analog.com/​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and the evaluation software to configure and collect data from the EVAL-CN0372-PMDZ Evaluation Board (**CN0372 Board**). The evaluation board also has PMOD and IMOD compatible headers which allows for connection to other processors or microcontrollers.+This user guide will discuss how to operate the [[adi>en/​design-center/​evaluation-hardware-and-software/​evaluation-boards-kits/​EVAL_SDP-PMOD.html#​eb-overview| SDP-PMD-IB1Z]],​ [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and the evaluation software to configure and collect data from the EVAL-CN0372-PMDZ Evaluation Board (**CN0372 Board**). The evaluation board also has PMOD and IMOD compatible headers which allows for connection to other processors or microcontrollers.
  
-A complete design support package for the [[adi>​EVAL-CN0372-PMDZ]] evaluation board containing schematics, layouts (native and Gerber), and bill-of-materials can be found at: [[http://​www.analog.com/​CN0372-DesignSupport|CN0372-DesignSupport]].+A complete design support package for the [[adi>​EVAL-CN0372-PMDZ]] evaluation board containing schematics, layouts (native and Gerber), and bill-of-materials can be found at: [[adi>CN0372-DesignSupport|CN0372-DesignSupport]].
  
 {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0372:​1.png?​direct&​600|}} {{:​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0372:​1.png?​direct&​600|}}
resources/eval/user-guides/circuits-from-the-lab/cn0372.txt · Last modified: 03 Jan 2021 22:03 by Robin Getz