This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0371 [17 Jun 2015 19:59] – [CN-0371 Software User Guide] Walt Kester | resources:eval:user-guides:circuits-from-the-lab:cn0371 [29 Jul 2021 07:57] (current) – Hardware Registration Harvey John De Chavez | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== CN-0371 Software | ====== CN-0371 Software | ||
===== Overview ===== | ===== Overview ===== | ||
- | [[http:// | + | [[adi>CN0371|CN-0371]] is a complete linear variable differential transformer (LVDT) signal conditioning circuit that can accurately measure linear position or linear displacement from a mechanical reference. Synchronous demodulation in the analog domain is used to extract the position information and provides immunity to external noise. A 24-bit sigma-delta ADC digitizes the position output for high accuracy. |
- | LVDTs utilize electromagnetic coupling between the movable core and the coil assembly. This contactless (and hence frictionless) operation is a primary reason why they are widely used in aerospace, process controls, robotics, nuclear, chemical plants, hydraulics, power turbines, and other applications where operating environments can be hostile and long life and high reliability are required. | + | LVDTs utilize electromagnetic coupling between the movable core and the coil assembly. This contactless (and therefore |
The entire circuit, including the LVDT excitation signal, consumes only 10 mW of power. The circuit excitation frequency and output data rates are SPI programmable. The system has a programmable bandwidth versus dynamic range trade-off. It supports bandwidths of over 1 kHz, and at a bandwidth of 20 Hz, the circuit has a dynamic range of 100 dB, making it ideal for precision industrial position and gauging applications. | The entire circuit, including the LVDT excitation signal, consumes only 10 mW of power. The circuit excitation frequency and output data rates are SPI programmable. The system has a programmable bandwidth versus dynamic range trade-off. It supports bandwidths of over 1 kHz, and at a bandwidth of 20 Hz, the circuit has a dynamic range of 100 dB, making it ideal for precision industrial position and gauging applications. | ||
This circuit note discusses the design steps needed to optimize the circuit shown in Figure 1 for a specific bandwidth including noise analysis and component selection considerations. | This circuit note discusses the design steps needed to optimize the circuit shown in Figure 1 for a specific bandwidth including noise analysis and component selection considerations. | ||
- | This user guide will discuss how to use the evaluation software to collect data from the [[http:// | + | This user guide will discuss how to use the evaluation software to collect data from the [[adi>EVAL-CN0371-SDPZ|EVAL-CN0371-SDPZ]] Evaluation Board **(CN-0371 Board)** |
{{: | {{: | ||
Line 12: | Line 12: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
- | * [[http:// | + | * [[adi>CN0371|EVAL-CN0371-SDPZ]] Evaluation Board (**CN-0371 Board**) |
- | * [[http:// | + | * [[adi> |
* [[ftp:// | * [[ftp:// | ||
* PC with the following //Minimum Requirements// | * PC with the following //Minimum Requirements// | ||
Line 23: | Line 23: | ||
* USB type A to USB type mini-B cable | * USB type A to USB type mini-B cable | ||
===== General Setup ===== | ===== General Setup ===== | ||
- | * The [[http:// | + | * The [[adi>EVAL-CN0371-SDPZ|EVAL-CN0371-SDPZ]] **(CN-0371 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector |
- | * The [[http:// | + | * The [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** powers the [[adi>CN0371|EVAL-CN0371-SDPZ]] **(CN-0371 Board)** via the DC barrel jack |
- | * The [[http:// | + | * The [[adi> |
\\ \\ {{: | \\ \\ {{: | ||
Line 41: | Line 41: | ||
===== Connecting the Hardware ===== | ===== Connecting the Hardware ===== | ||
- | - Connect the [[http:// | + | - Connect the [[adi> |
- | - Connect **P3** of the [[http:// | + | - Connect **P3** of the [[adi>EVAL-CN0371-SDPZ|EVAL-CN0371-SDPZ]] **(CN-0371 Board)** to **CON A** of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** |
- | - Connect the USB cable to **J1** of the [[http:// | + | - Connect the USB cable to **J1** of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)**\\ \\ {{: |
---- | ---- | ||
Line 80: | Line 80: | ||
* Output Data rate is the calculated ADC data rate. It is equal to 4800/(Data Rate Divider). | * Output Data rate is the calculated ADC data rate. It is equal to 4800/(Data Rate Divider). | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ |