This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0371 [19 Feb 2015 15:40] – [General Setup] Walt Kester | resources:eval:user-guides:circuits-from-the-lab:cn0371 [29 Jul 2021 07:57] (current) – Hardware Registration Harvey John De Chavez | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== CN-0371 Software User Guide====== | + | ====== CN-0371 Software |
===== Overview ===== | ===== Overview ===== | ||
- | [[http:// | + | [[adi>CN0371|CN-0371]] is a complete linear variable differential transformer (LVDT) signal conditioning circuit that can accurately measure linear position or linear displacement from a mechanical reference. Synchronous demodulation in the analog domain is used to extract the position information and provides immunity to external noise. A 24-bit sigma-delta ADC digitizes the position output for high accuracy. |
- | LVDTs utilize electromagnetic coupling between the movable core and the coil assembly. This contactless (and hence frictionless) operation is a primary reason why they are widely used in aerospace, process controls, robotics, nuclear, chemical plants, hydraulics, power turbines, and other applications where operating environments can be hostile and long life and high reliability are required. | + | LVDTs utilize electromagnetic coupling between the movable core and the coil assembly. This contactless (and therefore |
The entire circuit, including the LVDT excitation signal, consumes only 10 mW of power. The circuit excitation frequency and output data rates are SPI programmable. The system has a programmable bandwidth versus dynamic range trade-off. It supports bandwidths of over 1 kHz, and at a bandwidth of 20 Hz, the circuit has a dynamic range of 100 dB, making it ideal for precision industrial position and gauging applications. | The entire circuit, including the LVDT excitation signal, consumes only 10 mW of power. The circuit excitation frequency and output data rates are SPI programmable. The system has a programmable bandwidth versus dynamic range trade-off. It supports bandwidths of over 1 kHz, and at a bandwidth of 20 Hz, the circuit has a dynamic range of 100 dB, making it ideal for precision industrial position and gauging applications. | ||
This circuit note discusses the design steps needed to optimize the circuit shown in Figure 1 for a specific bandwidth including noise analysis and component selection considerations. | This circuit note discusses the design steps needed to optimize the circuit shown in Figure 1 for a specific bandwidth including noise analysis and component selection considerations. | ||
- | This user guide will discuss how to use the evaluation software to collect data from the [[http:// | + | This user guide will discuss how to use the evaluation software to collect data from the [[adi>EVAL-CN0371-SDPZ|EVAL-CN0371-SDPZ]] Evaluation Board **(CN-0371 Board)** |
{{: | {{: | ||
Line 12: | Line 12: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
- | * [[http:// | + | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] Controller Board (**SDP-B Board**) |
- | * [[http:// | + | * [[adi>CN0371|EVAL-CN0371-SDPZ]] Evaluation Board (**CN-0371 Board**) |
- | * [[http:// | + | * [[adi> |
* [[ftp:// | * [[ftp:// | ||
* PC with the following //Minimum Requirements// | * PC with the following //Minimum Requirements// | ||
Line 23: | Line 23: | ||
* USB type A to USB type mini-B cable | * USB type A to USB type mini-B cable | ||
===== General Setup ===== | ===== General Setup ===== | ||
- | * The [[http:// | + | * The [[adi>EVAL-CN0371-SDPZ|EVAL-CN0371-SDPZ]] **(CN-0371 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector |
- | * The [[http:// | + | * The [[adi>EVAL-CFTL-6V-PWRZ|EVAL-CFTL-6V-PWRZ]] **(+6V DC Power Supply)** powers the [[adi>CN0371|EVAL-CN0371-SDPZ]] **(CN-0371 Board)** via the DC barrel jack |
- | * The [[http:// | + | * The [[adi> |
\\ \\ {{: | \\ \\ {{: | ||
Line 31: | Line 31: | ||
===== Installing the Software ===== | ===== Installing the Software ===== | ||
- | - Extract the file **CN0371 Eval Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%> | + | - Extract the file **CN0371 Eval Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%> |
- | - Click **Next** to view the installation review page\\ \\ {{: | + | - Click **Next** to view the installation review page\\ \\ {{: |
- | - Click **Next** to start the installation\\ \\ {{: | + | - Click **Next** to start the installation\\ \\ {{: |
- | - Upon completion of the installation of the **CN-0371 Evaluation Software**, the installer for the **ADI SDP Drivers** will execute.\\ \\ <WRAP left tip round box 60%> | + | - Upon completion of the installation of the **CN-0371 Evaluation Software**, the installer for the **ADI SDP Drivers** will execute.\\ \\ <WRAP left tip round box 60%> |
- | - Press **“Next”** to set the installation location for the **SDP Drivers**.\\ \\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C: | + | - Press **“Next”** to set the installation location for the **SDP Drivers**.\\ \\ <WRAP left round tip 50%>It is recommended that you install the drivers to the default directory path \\ **C: |
- Press **“Next”** to install the **SDP Drivers** and complete the installation of all software. | - Press **“Next”** to install the **SDP Drivers** and complete the installation of all software. | ||
Line 41: | Line 41: | ||
===== Connecting the Hardware ===== | ===== Connecting the Hardware ===== | ||
- | - Connect the [[http:// | + | - Connect the [[adi> |
- | - Connect **P3** of the [[http:// | + | - Connect **P3** of the [[adi>EVAL-CN0371-SDPZ|EVAL-CN0371-SDPZ]] **(CN-0371 Board)** to **CON A** of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** |
- | - Connect the USB cable to **J1** of the [[http:// | + | - Connect the USB cable to **J1** of the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)**\\ \\ {{: |
---- | ---- | ||
Line 49: | Line 49: | ||
===== Using the Evaluation Software ===== | ===== Using the Evaluation Software ===== | ||
==== Linearity and Calibration Tabs ==== | ==== Linearity and Calibration Tabs ==== | ||
- | {{: | + | {{: |
-**Displacement Display** | -**Displacement Display** | ||
* The upper left hand corner shows the current measurement displacement in terms of voltage (V) and distance in millimeters (MM). In order to get accurate measurements, | * The upper left hand corner shows the current measurement displacement in terms of voltage (V) and distance in millimeters (MM). In order to get accurate measurements, | ||
Line 66: | Line 66: | ||
==== Live Measurement and Noise Data Tabs ==== | ==== Live Measurement and Noise Data Tabs ==== | ||
- | {{: | + | {{: |
-**Live Measurement Chart** | -**Live Measurement Chart** | ||
* The Live measurement chart shows the last 200 ADC readings taken. The data shown is displayed in volts (left side vertical axis) and millimeters (right side vertical axis) based on the most recent calibration. | * The Live measurement chart shows the last 200 ADC readings taken. The data shown is displayed in volts (left side vertical axis) and millimeters (right side vertical axis) based on the most recent calibration. | ||
Line 73: | Line 73: | ||
---- | ---- | ||
==== Live Measurement and Settings Tabs ==== | ==== Live Measurement and Settings Tabs ==== | ||
- | {{: | + | {{: |
-**Settings Tab** | -**Settings Tab** | ||
* Full-Scale Range entry enables users to scale the voltage used for the ENOBs calculations in the Noise Data tab. | * Full-Scale Range entry enables users to scale the voltage used for the ENOBs calculations in the Noise Data tab. | ||
Line 80: | Line 80: | ||
* Output Data rate is the calculated ADC data rate. It is equal to 4800/(Data Rate Divider). | * Output Data rate is the calculated ADC data rate. It is equal to 4800/(Data Rate Divider). | ||
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ |