Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:circuits-from-the-lab:cn0370 [10 Jul 2018 20:17] – [Overview] Motoko Hunt | resources:eval:user-guides:circuits-from-the-lab:cn0370 [29 Jul 2021 07:56] (current) – Hardware Registration Harvey John De Chavez |
---|
[[adi>AD5542A]] is a single supply, 16-bit, serial input, voltage output DAC that is used to control the voltage to current conversion. [[adi>ADA4500-2]] is a single supply, dual low power amplifier with no zero-crossover distortion offering high linearity over the full, rail to rail common-mode input range. [[adi>ADA4500-2]] is used to buffer the reference voltage of the DAC and is also used in a buffer configuration to convert the voltage output of the DAC into current. [[adi>ADR4525]] is a high precision, low power, low noise voltage reference that is used to provide precise 2.5V reference voltage for the DAC. | [[adi>AD5542A]] is a single supply, 16-bit, serial input, voltage output DAC that is used to control the voltage to current conversion. [[adi>ADA4500-2]] is a single supply, dual low power amplifier with no zero-crossover distortion offering high linearity over the full, rail to rail common-mode input range. [[adi>ADA4500-2]] is used to buffer the reference voltage of the DAC and is also used in a buffer configuration to convert the voltage output of the DAC into current. [[adi>ADR4525]] is a high precision, low power, low noise voltage reference that is used to provide precise 2.5V reference voltage for the DAC. |
| |
This user guide will discuss how to use the [[adi>http://www.analog.com/EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]], [[adi>http://www.analog.com/SDP-PMD-IB1Z|SDP-I-PMOD]] and the evaluation software to be able to write and collect data from [[adi>EVAL-CN0370-SDPZ|EVAL-CN070-PMDZ]]. The evaluation board has provisions to read the output voltage of the DAC and an option to use an external supply voltage for the LED. | This user guide will discuss how to use the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]], [[adi>SDP-PMD-IB1Z|SDP-I-PMOD]] and the evaluation software to be able to write and collect data from [[adi>EVAL-CN0370-SDPZ|EVAL-CN070-PMDZ]]. The evaluation board has provisions to read the output voltage of the DAC and an option to use an external supply voltage for the LED. |
{{ :resources:eval:user-guides:circuits-from-the-lab:cn0370:cn0370.jpg?direct |}} | {{ :resources:eval:user-guides:circuits-from-the-lab:cn0370:cn0370.jpg?direct |}} |
===== Required Equipment ===== | ===== Required Equipment ===== |
| |
<WRAP round 80% download> | <WRAP round 80% download> |
[[http://www.analog.com/media/en/reference-design-documentation/design-integration-files/CN0370-DesignSupport.zip|EVAL-CN0370-PMDZ Design & Integration Files]] | [[adi>media/en/reference-design-documentation/design-integration-files/CN0370-DesignSupport.zip|EVAL-CN0370-PMDZ Design & Integration Files]] |
* Schematics | * Schematics |
* PCB Layout | * PCB Layout |
</WRAP> | </WRAP> |
| |
| =====Registration===== |
| <WRAP round tip 80% > |
| Receive software update notifications, documentation updates, view the latest videos, and more when you register your hardware. [[reg>EVAL-CN0370-PMDZ?&v=RevB|Register]] to receive all these great benefits and more! |
| </WRAP> |
//End of Document// | //End of Document// |