Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Next revision
Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0370 [15 Sep 2015 07:17]
Ramon Glenn Amparo created
resources:eval:user-guides:circuits-from-the-lab:cn0370 [29 Jul 2021 07:56] (current)
Harvey John De Chavez Hardware Registration
Line 4: Line 4:
 ===== Overview ===== ===== Overview =====
  
-CN0370 is a complete single supply 16-bit ​unbuffered voltage output ​DAC that maintains ±1 LSB integral and differential ​linearity by utilizing a CMOS DAC, which has a voltage ​to current conversion for precision control ​of current through an LED. It offers a solution ​for a highly linear, low noise solution for controlling ​current.+[[adi>CN0370]] is a complete single-supply, low noise LED current source driver controlled by a 16-bit ​digital-to-analog converter (DAC). The system ​maintains ±1 LSB integral and differential ​nonlinearity and has a 0.1 Hz to 10 Hz noise of less than 45 nA p-p for a full-scale output ​current ​of 20 mA.
  
-AD5542A is a single supply, 16-bit, serial input, voltage output DAC that is used to control the voltage to current conversion. ADA4500-2 is a single supply, dual low power amplifier with no zero-crossover distortion offering high linearity over the full, rail to rail common-mode input range. ADA4500-2 is used to buffer the reference voltage of the DAC and is also used in a buffer configuration to convert the voltage output of the DAC into current. ADR4525 is a high precision, low power, low noise voltage reference that is used to provide precise 2.5V reference voltage for the DAC.+[[adi>AD5542A]] is a single supply, 16-bit, serial input, voltage output DAC that is used to control the voltage to current conversion. ​[[adi>ADA4500-2]] is a single supply, dual low power amplifier with no zero-crossover distortion offering high linearity over the full, rail to rail common-mode input range. ​[[adi>ADA4500-2]] is used to buffer the reference voltage of the DAC and is also used in a buffer configuration to convert the voltage output of the DAC into current. ​[[adi>ADR4525]] is a high precision, low power, low noise voltage reference that is used to provide precise 2.5V reference voltage for the DAC.
  
-This user guide will discuss how to use the EVAL-SDP-CB1Z,​ SDP-I-PMOD and the evaluation software to be able to write and collect data from EVAL-CN070-PMDZ. The evaluation board has provisions to read the output voltage of the DAC and an option to use an external supply voltage for the LED.  +This user guide will discuss how to use the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]][[adi>​SDP-PMD-IB1Z|SDP-I-PMOD]] and the evaluation software to be able to write and collect data from [[adi>​EVAL-CN0370-SDPZ|EVAL-CN070-PMDZ]]. The evaluation board has provisions to read the output voltage of the DAC and an option to use an external supply voltage for the LED.  
-{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0370.jpg?​direct&​300 ​|}}+{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:cn0370:​cn0370.jpg?​direct |}}
 ===== Required Equipment ===== ===== Required Equipment =====
  
   * PC with a USB port and Windows XP or Windows Vista   * PC with a USB port and Windows XP or Windows Vista
-32-b(it), or Windows 7 (32-bit)+    * 32-b(it), or Windows 7 (32-bit)
   * EVAL-SDP-CB1Z SDP evaluation board   * EVAL-SDP-CB1Z SDP evaluation board
   * PMD-SDP-IB1Z interposer board   * PMD-SDP-IB1Z interposer board
   * EVAL-CN0370-PMDZ circuit evaluation board   * EVAL-CN0370-PMDZ circuit evaluation board
   * CN-0370 evaluation software:   * CN-0370 evaluation software:
-ftp://​ftp.analog.com/​pub/​cftl/​CN0370/​+    * ftp://​ftp.analog.com/​pub/​cftl/​CN0370/​
   * Power supply: 6 V wall wart.   * Power supply: 6 V wall wart.
   * Agilent 34401A Multimeter or equivalent.   * Agilent 34401A Multimeter or equivalent.
Line 25: Line 25:
 ===== General Setup ===== ===== General Setup =====
  
- +{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0370:​cn0370-1.1.png?​direct |}}
   * Connect the 120-pin connector J4 on the PMD-SDP-IB1Z interposer board to the connector marked CON A on the EVAL-SDP-CB1Z (SDP) evaluation board. Shunt on JP1 to be place on the +5.0V configuration. ​   * Connect the 120-pin connector J4 on the PMD-SDP-IB1Z interposer board to the connector marked CON A on the EVAL-SDP-CB1Z (SDP) evaluation board. Shunt on JP1 to be place on the +5.0V configuration. ​
 +{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0370:​cn0370-2.jpg?​direct |}}
   * Connect the EVAL-CN0370-PMDZ to the PMOD connector J3.    * Connect the EVAL-CN0370-PMDZ to the PMOD connector J3. 
-  ​* Connect a +6V wall wart supply to the connector J1 of the interposer board. ​+{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0370:​cn0370-3.png?​direct |}} 
 +  ​* Connect a +6V wall wart supply to the connector J1 of the interposer board. 
 +{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0370:​cn0370-4.png?​direct |}}
   * The USB cable is used to connect EVAL-SDP-CB1Z to the PC.    * The USB cable is used to connect EVAL-SDP-CB1Z to the PC. 
-  ​* LED supply is shorted by a shunt to VPMOD by default.+{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0370:​eval-cn0370-pmdz-1.jpg?​direct |}} 
 +  ​LED_SUPPLY is the supply for the LED. It can be taken from the PMOD supply or an external voltage ​supply,VEXT. It is shorted by a shunt to PMOD by default.
   * Test point VCC and AGDN are used to take voltage measurements. ​   * Test point VCC and AGDN are used to take voltage measurements. ​
-  * JP1 on SDP-I-PMOD is shorted by a shunt on +5.0V configuration 
   * VEXT is used to supply an external voltage to the LED supply (Input range: +20max).   * VEXT is used to supply an external voltage to the LED supply (Input range: +20max).
  
 ===== Installing the Software ===== ===== Installing the Software =====
- +{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0370:​sw-1.png?​direct |}} 
-  * Extract the file CN0370_Evaluation_Software.zip and open the file setup.exe ​+  * Extract the file CN0370_Evaluation_Software.zip and open the file setup.exe 
 +{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0370:​sw-1.png?​direct |}}
   * Click Next to view the installation review page    * Click Next to view the installation review page 
 +{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0370:​sw-2.png?​direct |}} 
   * Click Next to begin the installation ​   * Click Next to begin the installation ​
 +{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0370:​sw-3.png?​direct |}}
   * Upon completion of the installation of the CN-0370 Evaluation Software, the installer for the ADI SDP Drivers will execute. ​   * Upon completion of the installation of the CN-0370 Evaluation Software, the installer for the ADI SDP Drivers will execute. ​
 +{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0370:​sw-4.png?​direct |}}
   * Click Next to set the installation location for the SDP Drivers ​   * Click Next to set the installation location for the SDP Drivers ​
 +{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0370:​sw-5.png?​direct |}}
   * Press Install to install the SDP Drivers and complete the installation of all software. Click Close when done.   * Press Install to install the SDP Drivers and complete the installation of all software. Click Close when done.
-  *  
 ===== Using the Evaluation Software ===== ===== Using the Evaluation Software =====
    
 ==== Main Tab ==== ==== Main Tab ====
 +{{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0370:​sw-gui.png?​direct |}}
   - Write data   - Write data
-This button is used to write the data into the DAC+     ​* ​This button is used to write the data into the DAC
   - Input Mode   - Input Mode
-  ​* This is a selector where the user can choose the input mode of changing the amount of current or changing the actual DAC code being written +    ​* This is a selector where the user can choose the input mode of changing the amount of current or changing the actual DAC code being written 
-  * Input Current Mode- the amount of current desired for the LED is adjusted and by pushing the Write Data button writes the data into the board. +    * Input Current Mode- the amount of current desired for the LED is adjusted and by pushing the Write Data button writes the data into the board. 
-  * Input Code Mode- the exact code is written on the Code box, and the amount of current output is automatically adjusted by pushing the Write Data button.+    * Input Code Mode- the exact code is written on the Code box, and the amount of current output is automatically adjusted by pushing the Write Data button.
   - External Resistor   - External Resistor
-  ​* Enable the external resistor if the resistor on R_LIMIT has been changed+    ​* Enable the external resistor if the resistor on R_LIMIT has been changed
   - Iout   - Iout
-  ​* This control will enable the user to change the amount of current flowing through the LED+    ​* This control will enable the user to change the amount of current flowing through the LED
   - R_limit   - R_limit
-  ​* This is the value of the resistor that limits the amount of current ​ through the LED, it is set to a default value of 124Ω+    ​* This is the value of the resistor that limits the amount of current ​ through the LED, it is set to a default value of 124Ω
  
 ==== Writing data ==== ==== Writing data ====
Line 77: Line 84:
   - Write the exact code to be written in the Code text box.   - Write the exact code to be written in the Code text box.
   - Push the Write Data button to write the code to the board.   - Push the Write Data button to write the code to the board.
 +
 +===== Schematic, PCB Layout, Bill of Materials =====
 +
 +<WRAP round 80% download>​
 +[[adi>​media/​en/​reference-design-documentation/​design-integration-files/​CN0370-DesignSupport.zip|EVAL-CN0370-PMDZ Design & Integration Files]]
 +  * Schematics ​
 +  * PCB Layout ​
 +  * Bill of Materials ​
 +  * Allegro Layout Files
 +</​WRAP>​
 +
 +=====Registration===== ​
 +<WRAP round tip 80% >
 +Receive software update notifications,​ documentation updates, view the latest videos, and more when you register your hardware. ​ [[reg>​EVAL-CN0370-PMDZ?&​v=RevB|Register]] to receive all these great benefits and more!
 +</​WRAP>​
 +//End of Document//
resources/eval/user-guides/circuits-from-the-lab/cn0370.1442294220.txt.gz · Last modified: 15 Sep 2015 07:17 by Ramon Glenn Amparo