This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0368 [30 Mar 2015 21:22] – [Multiple Temperature Calibration] Neil Wilson | resources:eval:user-guides:circuits-from-the-lab:cn0368 [30 Mar 2015 21:37] – [Overview] Neil Wilson | ||
---|---|---|---|
Line 6: | Line 6: | ||
The circuit is ideal for applications where high speed, accurate, non-contact angle and length measurements are critical such as brushless DC motor control. | The circuit is ideal for applications where high speed, accurate, non-contact angle and length measurements are critical such as brushless DC motor control. | ||
+ | {{ : | ||
===== General Setup ===== | ===== General Setup ===== | ||
*One [[http:// | *One [[http:// |