Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:user-guides:circuits-from-the-lab:cn0364 [03 Jan 2021 21:55]
Robin Getz fix links
resources:eval:user-guides:circuits-from-the-lab:cn0364 [06 Jan 2021 08:28] (current)
Ioana Chelaru Fixed bad link for EVAL-CN0364-SDPZ and removed reference for EVAL-SDP-CB1Z
Line 8: Line 8:
 This user guide will discuss how to use the [[adi>​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and evaluation software to configure and collect data from the EVAL-CN0364-SDPZ Evaluation Board **(CN-0364 Board)**. The evaluation board also has PMOD compatible headers for connection to other processors or microcontrollers. This user guide will discuss how to use the [[adi>​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and evaluation software to configure and collect data from the EVAL-CN0364-SDPZ Evaluation Board **(CN-0364 Board)**. The evaluation board also has PMOD compatible headers for connection to other processors or microcontrollers.
  
-A complete design support package for the [[adi>​EVAL-CN0364-SDPZ]] evaluation board containing schematics, layouts (native and Gerber), and bill-of-materials can be found at: [[adi>​CN0364-DesignSupport|CN0364-DesignSupport]].+A complete design support package for the [[adi>CN0364|EVAL-CN0364-SDPZ]] evaluation board containing schematics, layouts (native and Gerber), and bill-of-materials can be found at: [[adi>​CN0364-DesignSupport|CN0364-DesignSupport]].
  
 {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0364:​cn0364.jpg?​nolink&​300 |}} {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0364:​cn0364.jpg?​nolink&​300 |}}
Line 15: Line 15:
  
 ===== Required Equipment ===== ===== Required Equipment =====
-  * [[adi>EVAL-CN0364-SDPZ|EVAL-CN0364-SDPZ Evaluation Board]] +  * [[adi>​CN0364|EVAL-CN0364-SDPZ Evaluation Board]] 
-  * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] ​Controller Board (**SDP-B Board**)+  * EVAL-SDP-CB1Z Controller Board (**SDP-B Board**)
   * DC Power Supply (+12V to +24V)   * DC Power Supply (+12V to +24V)
   * Precision voltage and current source (for input)   * Precision voltage and current source (for input)
Line 31: Line 31:
 ===== General Setup ===== ===== General Setup =====
 {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0364:​setup-1.png?​nolink&​300 |}} {{ :​resources:​eval:​user-guides:​circuits-from-the-lab:​cn0364:​setup-1.png?​nolink&​300 |}}
-  * The [[adi>EVAL-CN0364-SDPZ|EVAL-CN0364-SDPZ]] **(CN-0364 Board)** connects to the [[adi>​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector+  * The [[adi>​CN0364|EVAL-CN0364-SDPZ]] **(CN-0364 Board)** connects to the [[adi>​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector
   * The [[adi>​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable.   * The [[adi>​EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable.
   * Header **P10** is a PMOD compatible SPI header - allows for communication to the ADC   * Header **P10** is a PMOD compatible SPI header - allows for communication to the ADC
resources/eval/user-guides/circuits-from-the-lab/cn0364.1609707353.txt.gz · Last modified: 03 Jan 2021 21:55 by Robin Getz