This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:cn0364 [14 Jan 2015 15:39] – [Software Control and Indicator Descriptions] Derrick Hartmann | resources:eval:user-guides:circuits-from-the-lab:cn0364 [06 Jan 2021 08:28] (current) – Fixed bad link for EVAL-CN0364-SDPZ and removed reference for EVAL-SDP-CB1Z Ioana Chelaru | ||
---|---|---|---|
Line 6: | Line 6: | ||
The [[ADI> | The [[ADI> | ||
- | This user guide will discuss how to use the [[http:// | + | This user guide will discuss how to use the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] and evaluation software to configure and collect data from the EVAL-CN0364-SDPZ Evaluation Board **(CN-0364 Board)**. The evaluation board also has PMOD compatible headers for connection to other processors or microcontrollers. |
- | A complete design support package for the [[adi> | + | A complete design support package for the [[adi>CN0364|EVAL-CN0364-SDPZ]] evaluation board containing schematics, layouts (native and Gerber), and bill-of-materials can be found at: [[adi>CN0364-DesignSupport|CN0364-DesignSupport]]. |
{{ : | {{ : | ||
Line 15: | Line 15: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
- | * [[adi>EVAL-CN0364-SDPZ|EVAL-CN0364-SDPZ Evaluation Board]] | + | * [[adi> |
- | * [[http:// | + | * EVAL-SDP-CB1Z Controller Board (**SDP-B Board**) |
* DC Power Supply (+12V to +24V) | * DC Power Supply (+12V to +24V) | ||
* Precision voltage and current source (for input) | * Precision voltage and current source (for input) | ||
- | * [[ftp:// | + | * [[ftp:// |
* PC with the following //Minimum Requirements// | * PC with the following //Minimum Requirements// | ||
* Windows Vista/7 (32-bit) | * Windows Vista/7 (32-bit) | ||
Line 31: | Line 31: | ||
===== General Setup ===== | ===== General Setup ===== | ||
{{ : | {{ : | ||
- | * The [[http:// | + | * The [[adi>CN0364|EVAL-CN0364-SDPZ]] **(CN-0364 Board)** connects to the [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** via the 120-Pin connector |
- | * The [[http:// | + | * The [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] **(SDP-B Board)** connects to the PC via the USB cable. |
* Header **P10** is a PMOD compatible SPI header - allows for communication to the ADC | * Header **P10** is a PMOD compatible SPI header - allows for communication to the ADC | ||
* Header **P11** is a PMOD compatible UART header - allows for communication to the HART modem | * Header **P11** is a PMOD compatible UART header - allows for communication to the HART modem | ||
Line 38: | Line 38: | ||
* Terminal blocks **P1**, | * Terminal blocks **P1**, | ||
* Terminal blocks **P5**, | * Terminal blocks **P5**, | ||
+ | |||
+ | See image for terminal block assignments: | ||
+ | {{ : | ||
**Jumper Settings** | **Jumper Settings** | ||
Line 160: | Line 163: | ||
- Click the **OK Button**. | - Click the **OK Button**. | ||
<WRAP center round info 60%>\\ The software saves the spreadsheet file as ASCII text with columns separated by tabs</ | <WRAP center round info 60%>\\ The software saves the spreadsheet file as ASCII text with columns separated by tabs</ | ||
+ | |||
+ | ---- | ||
+ | |||
+ | ===== More Information and Useful Links ===== | ||
+ | * [[ftp:// | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> | ||
+ | * [[ADI> |